Using CDC Class device with Linux

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Using CDC Class device with Linux

ソリューションへジャンプ
7,906件の閲覧回数
Nouchi
Senior Contributor II

Hello,

 

I'm using MQX3.5.1 CDC virtual com exemple program with M52259demo board, working fine with windows, and I would like to know how to use it with ubuntu system.

I'm looking for exemples.

 

Emmanuel

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 解決策
4,637件の閲覧回数
Nouchi
Senior Contributor II

Hello,

 

I found a solution to makes my M52259DEMO Kit to be recognized as ttyACM0, by changing a definition in g_config_descriptor table:

 

//#define CIC_PROTOCOL_CODE                NO_CLASS_SPECIFIC_PROTOCOL#define CIC_PROTOCOL_CODE                AT_250_PROTOCOL

It seems Linux USB enumerator needs some protocol definition.

This change doesn't affect behaviour with windows.

I performed some successful test with hyperterminal and minicom

 

 

元の投稿で解決策を見る

0 件の賞賛
返信
5 返答(返信)
4,637件の閲覧回数
Nouchi
Senior Contributor II

Hello,

 

I add some logs informations.

When I plug M52259demo USB<->232 bridge I've got :

 

[  780.570063] usb 9-1: new full speed USB device using ohci_hcd and address 2
[  780.806436] usb 9-1: configuration #1 chosen from 1 choice

 and nothing else, no device created.

 

I tried to plug FTDI chip:

 

[ 1157.490823] usb 2-5.4: new full speed USB device using ehci_hcd and address 7
[ 1157.607627] usb 2-5.4: configuration #1 chosen from 1 choice
[ 1157.610725] ftdi_sio 2-5.4:1.0: FTDI USB Serial Device converter detected
[ 1157.610921] usb 2-5.4: Detected FT232RL
[ 1157.610927] usb 2-5.4: Number of endpoints 2
[ 1157.610933] usb 2-5.4: Endpoint 1 MaxPacketSize 64
[ 1157.610940] usb 2-5.4: Endpoint 2 MaxPacketSize 64
[ 1157.610945] usb 2-5.4: Setting MaxPacketSize 64
[ 1157.611531] usb 2-5.4: FTDI USB Serial Device converter now attached to ttyUSB0

I can see ftdi_sio module loaded and ttyUSB0 device added, so what is missing to get new tty device with USB-232 bridge demo?

I also tried to load usbserial  module vith VID=0x2504 & PID=0x0300 without any success.

 

 

0 件の賞賛
返信
4,637件の閲覧回数
JuroV
NXP Employee
NXP Employee

If you say that new module is dynamically loaded, then you should be able to use new port. What happens when fopen-ing it?

0 件の賞賛
返信
4,637件の閲覧回数
Nouchi
Senior Contributor II

Hello,

 

I can't do fopen, because there's no ttyUSB device created, because no module loaded.

lsusb gives:

 

Bus 009 Device 005: ID 2504:0300

 We can see there's no identification string, seem's to be weird?

 

With an FTDI and TI TUSB device it gives :

 

Bus 008 Device 003: ID 0403:6001 Future Technology Devices International, Ltd FT232 USB-Serial (UART) IC
Bus 009 Device 003: ID 0451:3410 Texas Instruments, Inc. TUSB3410 Microcontroller

 

Only, usbserial ftd_sio and TI module were loaded.

 

lsmod
ftdi_sio               37981  0
ti_usb_3410_5052       26227  0
usbserial              39067  2 ti_usb_3410_5052,ftdi_sio

 

With FTDI devices it load ftdi_sio module, with TI TUSB chip it load ti_usb_3410_5052 module

 

Which (generic?)module should be loaded with usbserial?

 

 

Emmanuel

 

 

 

 

0 件の賞賛
返信
4,636件の閲覧回数
Nouchi
Senior Contributor II

lsusb -v

 

Bus 009 Device 002: ID 2504:0300  Device Descriptor:  bLength                18  bDescriptorType         1  bcdUSB               2.00  bDeviceClass            2 Communications  bDeviceSubClass         0   bDeviceProtocol         0   bMaxPacketSize0        64  idVendor           0x2504   idProduct          0x0300   bcdDevice            0.02  iManufacturer           1   iProduct                2   iSerial                 0   bNumConfigurations      1  Configuration Descriptor:    bLength                 9    bDescriptorType         2    wTotalLength           67    bNumInterfaces          2    bConfigurationValue     1    iConfiguration          0     bmAttributes         0xc0      Self Powered    MaxPower              100mA    Interface Descriptor:      bLength                 9      bDescriptorType         4      bInterfaceNumber        0      bAlternateSetting       0      bNumEndpoints           1      bInterfaceClass         2 Communications      bInterfaceSubClass      2 Abstract (modem)      bInterfaceProtocol      0 None      iInterface              0       CDC Header:        bcdCDC               1.10      CDC Call Management:        bmCapabilities       0x01          call management        bDataInterface          1      CDC ACM:        bmCapabilities       0x06          sends break          line coding and serial state      CDC Union:        bMasterInterface        0        bSlaveInterface         1       Endpoint Descriptor:        bLength                 7        bDescriptorType         5        bEndpointAddress     0x81  EP 1 IN        bmAttributes            3          Transfer Type            Interrupt          Synch Type               None          Usage Type               Data        wMaxPacketSize     0x0010  1x 16 bytes        bInterval              10    Interface Descriptor:      bLength                 9      bDescriptorType         4      bInterfaceNumber        1      bAlternateSetting       0      bNumEndpoints           2      bInterfaceClass        10 CDC Data      bInterfaceSubClass      0 Unused      bInterfaceProtocol      0       iInterface              0       Endpoint Descriptor:        bLength                 7        bDescriptorType         5        bEndpointAddress     0x82  EP 2 IN        bmAttributes            2          Transfer Type            Bulk          Synch Type               None          Usage Type               Data        wMaxPacketSize     0x0040  1x 64 bytes        bInterval               0      Endpoint Descriptor:        bLength                 7        bDescriptorType         5        bEndpointAddress     0x03  EP 3 OUT        bmAttributes            2          Transfer Type            Bulk          Synch Type               None          Usage Type               Data        wMaxPacketSize     0x0040  1x 64 bytes        bInterval               0can't get device qualifier: Operation not permittedcan't get debug descriptor: Operation not permittedcannot read device status, Operation not permitted (1)

 

 

0 件の賞賛
返信
4,637件の閲覧回数
Nouchi
Senior Contributor II

Hello,

 

I found a solution to makes my M52259DEMO Kit to be recognized as ttyACM0, by changing a definition in g_config_descriptor table:

 

//#define CIC_PROTOCOL_CODE                NO_CLASS_SPECIFIC_PROTOCOL#define CIC_PROTOCOL_CODE                AT_250_PROTOCOL

It seems Linux USB enumerator needs some protocol definition.

This change doesn't affect behaviour with windows.

I performed some successful test with hyperterminal and minicom

 

 

0 件の賞賛
返信