Unhandled Interrupt

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
4,509件の閲覧回数
netra
Contributor IV

I want to write a code so, that i can know in run time which task is having unhand led interrupt . so,that i can restart that task again.

I am using MQX 3.5.

Thanks,

netra

タグ(2)
1 解決策
2,951件の閲覧回数
JerryFan
NXP Employee
NXP Employee

MQX has a way to figure that issue out.  You can use _task_set_exception_handler to install a exception handler to capture what you want.Please refer the demo code below.

static void expt_frm_dump(pointer ext_frm_ptr)

{

  static char *expt_name[] = {

    "None",

    "Reset",

    "NMI",

    "HardFault",

    "MemManage",

    "BusFault",

    "UsageFault",

    "Rsvd",

    "Rsvd",

    "Rsvd",

    "SVCall",

    "Debug Monitor",

    "Rsvd",

    "PendSV",

    "SysTick"

  };

  uint_32 excpt_num = __get_PSR() & 0x1F;

  printf("Opps, bad thing happened.\n");

  if(excpt_num < 16){

    printf("The exception [%s] throw by TASK 0x%x\n",

         expt_name[excpt_num] , _task_get_id());

 

    printf("Dump the exception frame as :\n");

    printf("R0:\t0x%08x\n", *((uint_32 *)ext_frm_ptr));

    printf("R1:\t0x%08x\n", *((uint_32 *)ext_frm_ptr + 1));

    printf("R2:\t0x%08x\n", *((uint_32 *)ext_frm_ptr + 2));

    printf("R3:\t0x%08x\n", *((uint_32 *)ext_frm_ptr + 3));

    printf("R12:\t0x%08x\n", *((uint_32 *)ext_frm_ptr + 4));

    printf("LR:\t0x%08x\n", *((uint_32 *)ext_frm_ptr + 5));

    printf("PC:\t0x%08x\n", *((uint_32 *)ext_frm_ptr + 6));

    printf("PSR:\t0x%08x\n", *((uint_32 *)ext_frm_ptr + 7));

  }else{

    printf("The external interrupt %d occured while no handler to serve it.\n");

  }

}

void  task_exception_handler(_mqx_uint para, pointer stack_ptr)

{

#if 0

   __asm (

                "push {lr}        \n"

                "mrs r0, psp   \n"

                "bl    expt_frm_dump   \n"

                "pop {pc}       \n"

  );

#endif

    pointer expt_frm_ptr = (pointer)__get_PSP();

    expt_frm_dump(expt_frm_ptr);

}

void hello_task(unsigned long para)

{

  unsigned int *p_bad = (unsigned int *)0;

  printf("Hello, MQX\n");

  printf("Install the _int_exception_isr to replace the _int_default_isr\n");

  _int_install_exception_isr();

  /* Set the exception handler of the task */

  _task_set_exception_handler(_task_get_id(), task_exception_handler);

  *p = 0;     //This will issue a HardFault exception

  _task_block();

}

BTW, unhandeld interrupt should be definely avoided.

EDIT: Use C++ code highlight in the Advanced editor. Thanks! Message was edited by: Martin Kojtal

元の投稿で解決策を見る

3 返答(返信)
2,951件の閲覧回数
c0170
Senior Contributor III

Hello netra,

I am wondering about your intention. Could you please explain us why would you restart the task which causes an unhandled interrupt?

Regards,

0xc0170

0 件の賞賛
返信
2,951件の閲覧回数
drummer
Contributor IV

I was having a similar issue with a task that was aborting due to "unhandeld interrupt". I put a counter into the while(1) loop and waited for the exception to occur. The counter was always stopped at 4. So I cycled through 4 times and single stepped until it crashed. I kept my eye on any changes to file handles and discovered that an essential file handle was being changed .

I then used the watchpoint feature to see when the memory location was being changed. It ended up being another task that was writing the bad data.

2,952件の閲覧回数
JerryFan
NXP Employee
NXP Employee

MQX has a way to figure that issue out.  You can use _task_set_exception_handler to install a exception handler to capture what you want.Please refer the demo code below.

static void expt_frm_dump(pointer ext_frm_ptr)

{

  static char *expt_name[] = {

    "None",

    "Reset",

    "NMI",

    "HardFault",

    "MemManage",

    "BusFault",

    "UsageFault",

    "Rsvd",

    "Rsvd",

    "Rsvd",

    "SVCall",

    "Debug Monitor",

    "Rsvd",

    "PendSV",

    "SysTick"

  };

  uint_32 excpt_num = __get_PSR() & 0x1F;

  printf("Opps, bad thing happened.\n");

  if(excpt_num < 16){

    printf("The exception [%s] throw by TASK 0x%x\n",

         expt_name[excpt_num] , _task_get_id());

 

    printf("Dump the exception frame as :\n");

    printf("R0:\t0x%08x\n", *((uint_32 *)ext_frm_ptr));

    printf("R1:\t0x%08x\n", *((uint_32 *)ext_frm_ptr + 1));

    printf("R2:\t0x%08x\n", *((uint_32 *)ext_frm_ptr + 2));

    printf("R3:\t0x%08x\n", *((uint_32 *)ext_frm_ptr + 3));

    printf("R12:\t0x%08x\n", *((uint_32 *)ext_frm_ptr + 4));

    printf("LR:\t0x%08x\n", *((uint_32 *)ext_frm_ptr + 5));

    printf("PC:\t0x%08x\n", *((uint_32 *)ext_frm_ptr + 6));

    printf("PSR:\t0x%08x\n", *((uint_32 *)ext_frm_ptr + 7));

  }else{

    printf("The external interrupt %d occured while no handler to serve it.\n");

  }

}

void  task_exception_handler(_mqx_uint para, pointer stack_ptr)

{

#if 0

   __asm (

                "push {lr}        \n"

                "mrs r0, psp   \n"

                "bl    expt_frm_dump   \n"

                "pop {pc}       \n"

  );

#endif

    pointer expt_frm_ptr = (pointer)__get_PSP();

    expt_frm_dump(expt_frm_ptr);

}

void hello_task(unsigned long para)

{

  unsigned int *p_bad = (unsigned int *)0;

  printf("Hello, MQX\n");

  printf("Install the _int_exception_isr to replace the _int_default_isr\n");

  _int_install_exception_isr();

  /* Set the exception handler of the task */

  _task_set_exception_handler(_task_get_id(), task_exception_handler);

  *p = 0;     //This will issue a HardFault exception

  _task_block();

}

BTW, unhandeld interrupt should be definely avoided.

EDIT: Use C++ code highlight in the Advanced editor. Thanks! Message was edited by: Martin Kojtal