Unhandled Interrupt

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Unhandled Interrupt

Jump to solution
4,663 Views
netra
Contributor III

I want to write a code so, that i can know in run time which task is having unhand led interrupt . so,that i can restart that task again.

I am using MQX 3.5.

Thanks,

netra

Tags (2)
1 Solution
3,105 Views
JerryFan
NXP Employee
NXP Employee

MQX has a way to figure that issue out.  You can use _task_set_exception_handler to install a exception handler to capture what you want.Please refer the demo code below.

static void expt_frm_dump(pointer ext_frm_ptr)

{

  static char *expt_name[] = {

    "None",

    "Reset",

    "NMI",

    "HardFault",

    "MemManage",

    "BusFault",

    "UsageFault",

    "Rsvd",

    "Rsvd",

    "Rsvd",

    "SVCall",

    "Debug Monitor",

    "Rsvd",

    "PendSV",

    "SysTick"

  };

  uint_32 excpt_num = __get_PSR() & 0x1F;

  printf("Opps, bad thing happened.\n");

  if(excpt_num < 16){

    printf("The exception [%s] throw by TASK 0x%x\n",

         expt_name[excpt_num] , _task_get_id());

 

    printf("Dump the exception frame as :\n");

    printf("R0:\t0x%08x\n", *((uint_32 *)ext_frm_ptr));

    printf("R1:\t0x%08x\n", *((uint_32 *)ext_frm_ptr + 1));

    printf("R2:\t0x%08x\n", *((uint_32 *)ext_frm_ptr + 2));

    printf("R3:\t0x%08x\n", *((uint_32 *)ext_frm_ptr + 3));

    printf("R12:\t0x%08x\n", *((uint_32 *)ext_frm_ptr + 4));

    printf("LR:\t0x%08x\n", *((uint_32 *)ext_frm_ptr + 5));

    printf("PC:\t0x%08x\n", *((uint_32 *)ext_frm_ptr + 6));

    printf("PSR:\t0x%08x\n", *((uint_32 *)ext_frm_ptr + 7));

  }else{

    printf("The external interrupt %d occured while no handler to serve it.\n");

  }

}

void  task_exception_handler(_mqx_uint para, pointer stack_ptr)

{

#if 0

   __asm (

                "push {lr}        \n"

                "mrs r0, psp   \n"

                "bl    expt_frm_dump   \n"

                "pop {pc}       \n"

  );

#endif

    pointer expt_frm_ptr = (pointer)__get_PSP();

    expt_frm_dump(expt_frm_ptr);

}

void hello_task(unsigned long para)

{

  unsigned int *p_bad = (unsigned int *)0;

  printf("Hello, MQX\n");

  printf("Install the _int_exception_isr to replace the _int_default_isr\n");

  _int_install_exception_isr();

  /* Set the exception handler of the task */

  _task_set_exception_handler(_task_get_id(), task_exception_handler);

  *p = 0;     //This will issue a HardFault exception

  _task_block();

}

BTW, unhandeld interrupt should be definely avoided.

EDIT: Use C++ code highlight in the Advanced editor. Thanks! Message was edited by: Martin Kojtal

View solution in original post

3 Replies
3,105 Views
c0170
Senior Contributor III

Hello netra,

I am wondering about your intention. Could you please explain us why would you restart the task which causes an unhandled interrupt?

Regards,

0xc0170

0 Kudos
Reply
3,105 Views
drummer
Contributor IV

I was having a similar issue with a task that was aborting due to "unhandeld interrupt". I put a counter into the while(1) loop and waited for the exception to occur. The counter was always stopped at 4. So I cycled through 4 times and single stepped until it crashed. I kept my eye on any changes to file handles and discovered that an essential file handle was being changed .

I then used the watchpoint feature to see when the memory location was being changed. It ended up being another task that was writing the bad data.

3,106 Views
JerryFan
NXP Employee
NXP Employee

MQX has a way to figure that issue out.  You can use _task_set_exception_handler to install a exception handler to capture what you want.Please refer the demo code below.

static void expt_frm_dump(pointer ext_frm_ptr)

{

  static char *expt_name[] = {

    "None",

    "Reset",

    "NMI",

    "HardFault",

    "MemManage",

    "BusFault",

    "UsageFault",

    "Rsvd",

    "Rsvd",

    "Rsvd",

    "SVCall",

    "Debug Monitor",

    "Rsvd",

    "PendSV",

    "SysTick"

  };

  uint_32 excpt_num = __get_PSR() & 0x1F;

  printf("Opps, bad thing happened.\n");

  if(excpt_num < 16){

    printf("The exception [%s] throw by TASK 0x%x\n",

         expt_name[excpt_num] , _task_get_id());

 

    printf("Dump the exception frame as :\n");

    printf("R0:\t0x%08x\n", *((uint_32 *)ext_frm_ptr));

    printf("R1:\t0x%08x\n", *((uint_32 *)ext_frm_ptr + 1));

    printf("R2:\t0x%08x\n", *((uint_32 *)ext_frm_ptr + 2));

    printf("R3:\t0x%08x\n", *((uint_32 *)ext_frm_ptr + 3));

    printf("R12:\t0x%08x\n", *((uint_32 *)ext_frm_ptr + 4));

    printf("LR:\t0x%08x\n", *((uint_32 *)ext_frm_ptr + 5));

    printf("PC:\t0x%08x\n", *((uint_32 *)ext_frm_ptr + 6));

    printf("PSR:\t0x%08x\n", *((uint_32 *)ext_frm_ptr + 7));

  }else{

    printf("The external interrupt %d occured while no handler to serve it.\n");

  }

}

void  task_exception_handler(_mqx_uint para, pointer stack_ptr)

{

#if 0

   __asm (

                "push {lr}        \n"

                "mrs r0, psp   \n"

                "bl    expt_frm_dump   \n"

                "pop {pc}       \n"

  );

#endif

    pointer expt_frm_ptr = (pointer)__get_PSP();

    expt_frm_dump(expt_frm_ptr);

}

void hello_task(unsigned long para)

{

  unsigned int *p_bad = (unsigned int *)0;

  printf("Hello, MQX\n");

  printf("Install the _int_exception_isr to replace the _int_default_isr\n");

  _int_install_exception_isr();

  /* Set the exception handler of the task */

  _task_set_exception_handler(_task_get_id(), task_exception_handler);

  *p = 0;     //This will issue a HardFault exception

  _task_block();

}

BTW, unhandeld interrupt should be definely avoided.

EDIT: Use C++ code highlight in the Advanced editor. Thanks! Message was edited by: Martin Kojtal