USB host, Int Flash Release problem

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

USB host, Int Flash Release problem

2,067 次查看
tomaszk
Contributor II

Hi,

 

CW 7.1.2, MQX 3.4, M52259EVB

 

My USB host application is working fine in Debug Mode but there is a problem in Int Flash Release mode.

Every time when I insert the USB stick I got this error:

 

************************************************************************
Vendor Information:              Mass Storage Device
Product Identification: Flash Disk
Product Revision Level: 8.07
************************************************************************
Error while opening partition (UNKNOWN ERROR !!!)
Device removed, starting device cleanup
--->Closing MFS
--->Uninstalling
--->Uninstalling PM
--->Closing disk

 

After that I have to restart microcontroller to use USB again.

 

I've check my application, web_hvac and mfs_usb examples with freescale and kingston sticks so far.

 

 

Any ideas?

 

Regards,

tomaszk

 

标签 (1)
标记 (1)
0 项奖励
回复
1 回复

1,119 次查看
JuroV
NXP Employee
NXP Employee

Hello,

 

this is known bug of CodeWarrior compiler. I recommend to use CW7.2.

0 项奖励
回复