USB host, Int Flash Release problem

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

USB host, Int Flash Release problem

2,165件の閲覧回数
tomaszk
Contributor II

Hi,

 

CW 7.1.2, MQX 3.4, M52259EVB

 

My USB host application is working fine in Debug Mode but there is a problem in Int Flash Release mode.

Every time when I insert the USB stick I got this error:

 

************************************************************************
Vendor Information:              Mass Storage Device
Product Identification: Flash Disk
Product Revision Level: 8.07
************************************************************************
Error while opening partition (UNKNOWN ERROR !!!)
Device removed, starting device cleanup
--->Closing MFS
--->Uninstalling
--->Uninstalling PM
--->Closing disk

 

After that I have to restart microcontroller to use USB again.

 

I've check my application, web_hvac and mfs_usb examples with freescale and kingston sticks so far.

 

 

Any ideas?

 

Regards,

tomaszk

 

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 返信

1,217件の閲覧回数
JuroV
NXP Employee
NXP Employee

Hello,

 

this is known bug of CodeWarrior compiler. I recommend to use CW7.2.

0 件の賞賛
返信