USB OTG using MQX3.7

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
1,472件の閲覧回数
Mohsin455
Contributor IV

Hi,

 

       I am using MQX3.7 and K60N512 and have a few questions.

 

1) Does the MQX3.7 support OTG ?

 

2) Our custom board uses K60N512 and has got an OTG connector. Therefore how do we make the custom board select which mode. Do we have to use USB_ID or it is useless unless there is a support for OTG on MQX.

 

The same with USB OTG Interrupt select ? Is this also not used if OTG is not supported ?

 

Regards,

Mohsin

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 解決策
1,217件の閲覧回数
c0170
Senior Contributor III

Hi Mohsin455,

 

1. Does not support OTG.

2. Useless

3. Not used

 

Regards,

MartinK

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,218件の閲覧回数
c0170
Senior Contributor III

Hi Mohsin455,

 

1. Does not support OTG.

2. Useless

3. Not used

 

Regards,

MartinK

0 件の賞賛
返信