USB OTG using MQX3.7

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

USB OTG using MQX3.7

Jump to solution
1,479 Views
Mohsin455
Contributor IV

Hi,

 

       I am using MQX3.7 and K60N512 and have a few questions.

 

1) Does the MQX3.7 support OTG ?

 

2) Our custom board uses K60N512 and has got an OTG connector. Therefore how do we make the custom board select which mode. Do we have to use USB_ID or it is useless unless there is a support for OTG on MQX.

 

The same with USB OTG Interrupt select ? Is this also not used if OTG is not supported ?

 

Regards,

Mohsin

Labels (1)
Tags (1)
0 Kudos
Reply
1 Solution
1,224 Views
c0170
Senior Contributor III

Hi Mohsin455,

 

1. Does not support OTG.

2. Useless

3. Not used

 

Regards,

MartinK

View solution in original post

0 Kudos
Reply
1 Reply
1,225 Views
c0170
Senior Contributor III

Hi Mohsin455,

 

1. Does not support OTG.

2. Useless

3. Not used

 

Regards,

MartinK

0 Kudos
Reply