USB OTG using MQX3.7

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

USB OTG using MQX3.7

跳至解决方案
1,476 次查看
Mohsin455
Contributor IV

Hi,

 

       I am using MQX3.7 and K60N512 and have a few questions.

 

1) Does the MQX3.7 support OTG ?

 

2) Our custom board uses K60N512 and has got an OTG connector. Therefore how do we make the custom board select which mode. Do we have to use USB_ID or it is useless unless there is a support for OTG on MQX.

 

The same with USB OTG Interrupt select ? Is this also not used if OTG is not supported ?

 

Regards,

Mohsin

标签 (1)
标记 (1)
0 项奖励
回复
1 解答
1,221 次查看
c0170
Senior Contributor III

Hi Mohsin455,

 

1. Does not support OTG.

2. Useless

3. Not used

 

Regards,

MartinK

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,222 次查看
c0170
Senior Contributor III

Hi Mohsin455,

 

1. Does not support OTG.

2. Useless

3. Not used

 

Regards,

MartinK

0 项奖励
回复