USB Memory Stick Testing

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

USB Memory Stick Testing

16,856件の閲覧回数
rav
Contributor III

This is a place holder for feedback on all the USB sticks that are tested with MQX to ensure maximum compatibility.
1) Please post top USB Memory Stick Vendor for your region that need to be tested.
2) Please post the make/model/description of working and non-working USB sticks that you have tested.

 

A. Why Testing is Needed

Not all USB sticks conform to the same specification and there are small differences between them that can cause it not to work. Our goal is to debug the memory sticks that currently do not work and get them working with MQX if possible. 

 

B. How to Test

Make sure your disk is formatted to FAT16 or FAT32.
Download and run MQX Lab 2 (http://compass.freescale.net/doc/197259796/MQX_Labs.pdf). 
If you see something like this in HyperTerminal when you insert the USB stick:

Unable to open USB disk
Device removed, starting device cleanup
--->Closing MFS
--->uninstalling b:
--->Closing USB MFS

Then that means the USB stick was not properly mounted by MQX.

If this happens, open up the project in <mqx install directory>/usb/host/examples/mass/msc_commands/codewarrior/

Load and run the project with the USB stick unattached. Then with HyperTerminal open and connected, plug in the non-functioning USB stick. A test will run automatically upon insertion of the USB stick. Add a post in this thread with the output it generates, along with the exact make and model of the USB stick you are testing. 

Add a post for any USB stick that does work as well.  

 

C. Results

This will be continuously updated as people report which USB sticks work and do not work.

Working USB

- RiDATA 128MB (included with M5222EVB)
- Freescale silver-metal/black-plastic 64MB (included with M52259EVB)
- Freescale silver-metal/green-plastic 2GB - given away at FTF Americas 2008 and DFAE Training 2008
- Kingston DataTraveler DTI/1GB (http://www.kingston.com/flash/datatraveler.asp)

Not Working USB

-  

Message Edited by rav on 2009-05-28 07:39 PM
0 件の賞賛
返信
14 返答(返信)

7,913件の閲覧回数
yb
Contributor IV

Is there today a solution to add by ourself new USB stick to MQX ? What is the process to do it ?

This is a REAL problem for my customer which can use just a few of USB sticks (above 50% of commercial availability)...

The projet run under MQX 3.8.1

0 件の賞賛
返信

7,913件の閲覧回数
dspNeil
Contributor III

I have not found a single SanDisk drive that works!

 

Setup: CW10.2, MQX3.8, TWRK53, Project: msd_cmd_twrk53n512 (But my own program on my custom K53 board is where I first discovered the issue)

 

Results:

 

SanDisk 8GB Model: SDCZ6-8192RB, U3 Removed, Full Fresh FAT32 Format

=============START OF A NEW SESSION==================
VID = 0x0781, PID = 0x5406
Testing: GET MAX LUN Command...OK
Testing: TEST UNIT READY Command...OK
Testing: REQUEST SENSE Command...OK
Testing: INQUIRY Command...OK
Testing: REQUEST SENSE Command...OK
Testing: READ FORMAT CAPACITIES Command...OK
Testing: REQUEST SENSE Command...OK
Testing: READ CAPACITY Command...OK
Testing: REQUEST SENSE Command...OK
Testing: READ(10) Command...Unsupported by device (bStatus=0x1)
Testing: MODE SENSE Command...Unsupported by device (bStatus=0xfffffff9)
Testing: PREVENT-ALLOW MEDIUM REMOVAL Command...Unsupported by device (bStatus=0xfffffff9)
Testing: REQUEST SENSE Command...Unsupported by device (bStatus=0xfffffff9)
Testing: VERIFY Command...Unsupported by device (bStatus=0xfffffff9)
Testing: WRITE(10) Command...Unsupported by device (bStatus=0xfffffff9)
Testing: REQUEST SENSE Command...Unsupported by device (bStatus=0xfffffff9)
Testing: START-STOP UNIT Command...Unsupported by device (bStatus=0xfffffff9)

 

 

SanDisk Cruzer 4GB Model: SDCZ36-004G, FAT32, No U3

=============START OF A NEW SESSION==================
VID = 0x0781, PID = 0x5530
Testing: GET MAX LUN Command...OK
Testing: TEST UNIT READY Command...OK
Testing: REQUEST SENSE Command...OK
Testing: INQUIRY Command...OK
Testing: REQUEST SENSE Command...OK
Testing: READ FORMAT CAPACITIES Command...OK
Testing: REQUEST SENSE Command...OK
Testing: READ CAPACITY Command...OK
Testing: REQUEST SENSE Command...OK
Testing: READ(10) Command...Unsupported by device (bStatus=0x1)
Testing: MODE SENSE Command...Unsupported by device (bStatus=0xfffffff9)
Testing: PREVENT-ALLOW MEDIUM REMOVAL Command...Unsupported by device (bStatus=0xfffffff9)
Testing: REQUEST SENSE Command...Unsupported by device (bStatus=0xfffffff9)
Testing: VERIFY Command...Unsupported by device (bStatus=0xfffffff9)
Testing: WRITE(10) Command...Unsupported by device (bStatus=0xfffffff9)
Testing: REQUEST SENSE Command...Unsupported by device (bStatus=0xfffffff9)
Testing: START-STOP UNIT Command...Unsupported by device (bStatus=0xfffffff9)

 

 

SanDisk Cruzer 16GB Model: SDCZ36-016G, FAT32, No U3

=============START OF A NEW SESSION==================
VID = 0x0781, PID = 0x5530
Testing: GET MAX LUN Command...OK
Testing: TEST UNIT READY Command...OK
Testing: REQUEST SENSE Command...OK
Testing: INQUIRY Command...OK
Testing: REQUEST SENSE Command...OK
Testing: READ FORMAT CAPACITIES Command...Unsupported by device (bStatus=0x1)
Testing: REQUEST SENSE Command...Unsupported by device (bStatus=0xfffffff9)
Testing: READ CAPACITY Command...Unsupported by device (bStatus=0xfffffff9)
Testing: REQUEST SENSE Command...Unsupported by device (bStatus=0xfffffff9)
Testing: READ(10) Command...Unsupported by device (bStatus=0xfffffff9)
Testing: MODE SENSE Command...Unsupported by device (bStatus=0xfffffff9)
Testing: PREVENT-ALLOW MEDIUM REMOVAL Command...Unsupported by device (bStatus=0xfffffff9)
Testing: REQUEST SENSE Command...Unsupported by device (bStatus=0xfffffff9)
Testing: VERIFY Command...Unsupported by device (bStatus=0xfffffff9)
Testing: WRITE(10) Command...Unsupported by device (bStatus=0xfffffff9)
Testing: REQUEST SENSE Command...Unsupported by device (bStatus=0xfffffff9)
Testing: START-STOP UNIT Command...Unsupported by device (bStatus=0xfffffff9)

 

 

Promo Drive, ST U210 1G, FAT32, Single Partition

=============START OF A NEW SESSION==================
VID = 0x0dd8, PID = 0x1728
Testing: GET MAX LUN Command...OK
Testing: TEST UNIT READY Command...OK
Testing: REQUEST SENSE Command...Unsupported by device (bStatus=0x97)
Testing: INQUIRY Command...Unsupported by device (bStatus=0xfffffff9)
Testing: REQUEST SENSE Command...Unsupported by device (bStatus=0xfffffff9)
Testing: READ FORMAT CAPACITIES Command...Unsupported by device (bStatus=0xfffffff9)
Testing: REQUEST SENSE Command...Unsupported by device (bStatus=0xfffffff9)
Testing: READ CAPACITY Command...Unsupported by device (bStatus=0xfffffff9)
Testing: REQUEST SENSE Command...Unsupported by device (bStatus=0xfffffff9)
Testing: READ(10) Command...Unsupported by device (bStatus=0xfffffff9)
Testing: MODE SENSE Command...Unsupported by device (bStatus=0xfffffff9)
Testing: PREVENT-ALLOW MEDIUM REMOVAL Command...Unsupported by device (bStatus=0xfffffff9)
Testing: REQUEST SENSE Command...Unsupported by device (bStatus=0xfffffff9)
Testing: VERIFY Command...Unsupported by device (bStatus=0xfffffff9)
Testing: WRITE(10) Command...Unsupported by device (bStatus=0xfffffff9)
Testing: REQUEST SENSE Command...Unsupported by device (bStatus=0xfffffff9)
Testing: START-STOP UNIT Command...Unsupported by device (bStatus=0xfffffff9)

 

 

Kingston 32MB (Yes, MB) No Model Listed, FAT

=============START OF A NEW SESSION==================
VID = 0x04e8, PID = 0x0100
Testing: GET MAX LUN Command...OK
Testing: TEST UNIT READY Command...OK
Testing: REQUEST SENSE Command...OK
Testing: INQUIRY Command...OK
Testing: REQUEST SENSE Command...OK
Testing: READ FORMAT CAPACITIES Command...OK
Testing: REQUEST SENSE Command...OK
Testing: READ CAPACITY Command...OK
Testing: REQUEST SENSE Command...OK
Testing: READ(10) Command...OK
Testing: MODE SENSE Command...OK
Testing: PREVENT-ALLOW MEDIUM REMOVAL Command...OK
Testing: REQUEST SENSE Command...OK
Testing: VERIFY Command...OK
Testing: WRITE(10) Command...OK
Testing: REQUEST SENSE Command...OK
Testing: START-STOP UNIT Command...OK

 

 

Kingston DataTraveler 8GB DTI/8GB, FAT32

=============START OF A NEW SESSION==================
VID = 0x0951, PID = 0x1603
Testing: GET MAX LUN Command...OK
Testing: TEST UNIT READY Command...OK
Testing: REQUEST SENSE Command...OK
Testing: INQUIRY Command...OK
Testing: REQUEST SENSE Command...OK
Testing: READ FORMAT CAPACITIES Command...OK
Testing: REQUEST SENSE Command...OK
Testing: READ CAPACITY Command...OK
Testing: REQUEST SENSE Command...OK
Testing: READ(10) Command...OK
Testing: MODE SENSE Command...OK
Testing: PREVENT-ALLOW MEDIUM REMOVAL Command...OK
Testing: REQUEST SENSE Command...OK
Testing: VERIFY Command...OK
Testing: WRITE(10) Command...OK
Testing: REQUEST SENSE Command...OK
Testing: START-STOP UNIT Command...OK

 

 

Freescale Drive included with CW License, 16GB, FAT32

=============START OF A NEW SESSION==================
VID = 0x090c, PID = 0x1000
Testing: GET MAX LUN Command...OK
Testing: TEST UNIT READY Command...OK
Testing: REQUEST SENSE Command...OK
Testing: INQUIRY Command...OK
Testing: REQUEST SENSE Command...OK
Testing: READ FORMAT CAPACITIES Command...OK
Testing: REQUEST SENSE Command...OK
Testing: READ CAPACITY Command...OK
Testing: REQUEST SENSE Command...OK
Testing: READ(10) Command...OK
Testing: MODE SENSE Command...OK
Testing: PREVENT-ALLOW MEDIUM REMOVAL Command...OK
Testing: REQUEST SENSE Command...OK
Testing: VERIFY Command...OK
Testing: WRITE(10) Command...OK
Testing: REQUEST SENSE Command...OK
Testing: START-STOP UNIT Command...OK

 

 

Promo Drive, No Model, 128MB, FAT

 

=============START OF A NEW SESSION==================
VID = 0x13fe, PID = 0x1a00
Testing: GET MAX LUN Command...OK
Testing: TEST UNIT READY Command...OK
Testing: REQUEST SENSE Command...OK
Testing: INQUIRY Command...OK
Testing: REQUEST SENSE Command...OK
Testing: READ FORMAT CAPACITIES Command...OK
Testing: REQUEST SENSE Command...OK
Testing: READ CAPACITY Command...OK
Testing: REQUEST SENSE Command...OK
Testing: READ(10) Command...OK
Testing: MODE SENSE Command...OK
Testing: PREVENT-ALLOW MEDIUM REMOVAL Command...OK
Testing: REQUEST SENSE Command...OK
Testing: VERIFY Command...OK
Testing: WRITE(10) Command...OK
Testing: REQUEST SENSE Command...OK
Testing: START-STOP UNIT Command...OK

 

 

Promo Drive, No Model, 32MB, FAT

=============START OF A NEW SESSION==================
VID = 0x0ea0, PID = 0x6828
Testing: GET MAX LUN Command...OK
Testing: TEST UNIT READY Command...OK
Testing: REQUEST SENSE Command...OK
Testing: INQUIRY Command...OK
Testing: REQUEST SENSE Command...OK
Testing: READ FORMAT CAPACITIES Command...OK
Testing: REQUEST SENSE Command...OK
Testing: READ CAPACITY Command...OK
Testing: REQUEST SENSE Command...OK
Testing: READ(10) Command...OK
Testing: MODE SENSE Command...OK
Testing: PREVENT-ALLOW MEDIUM REMOVAL Command...OK
Testing: REQUEST SENSE Command...OK
Testing: VERIFY Command...OK
Testing: WRITE(10) Command...OK
Testing: REQUEST SENSE Command...OK
Testing: START-STOP UNIT Command...OK

 

 

Lexar 8GB Model: LJDTT8GB-000-1002N, FAT32

=============START OF A NEW SESSION==================
VID = 0x05dc, PID = 0xa813
Testing: GET MAX LUN Command...OK
Testing: TEST UNIT READY Command...OK
Testing: REQUEST SENSE Command...OK
Testing: INQUIRY Command...OK
Testing: REQUEST SENSE Command...OK
Testing: READ FORMAT CAPACITIES Command...OK
Testing: REQUEST SENSE Command...OK
Testing: READ CAPACITY Command...OK
Testing: REQUEST SENSE Command...OK
Testing: READ(10) Command...OK
Testing: MODE SENSE Command...OK
Testing: PREVENT-ALLOW MEDIUM REMOVAL Command...OK
Testing: REQUEST SENSE Command...OK
Testing: VERIFY Command...OK
Testing: WRITE(10) Command...OK
Testing: REQUEST SENSE Command...OK
Testing: START-STOP UNIT Command...OK

0 件の賞賛
返信

7,913件の閲覧回数
dspNeil
Contributor III

Today I found an old SanDisk drive that actually works, as well as one more drive that fails more commands than any others I've seen. Here are the results:

 

SanDisk Cruzer Micro 1.0 GB, Model: SDCZ6-1024, FAT format, No U3

=============START OF A NEW SESSION==================
VID = 0x0781, PID = 0x5406
Testing: GET MAX LUN Command...OK
Testing: TEST UNIT READY Command...OK
Testing: REQUEST SENSE Command...OK
Testing: INQUIRY Command...OK
Testing: REQUEST SENSE Command...OK
Testing: READ FORMAT CAPACITIES Command...OK
Testing: REQUEST SENSE Command...OK
Testing: READ CAPACITY Command...OK
Testing: REQUEST SENSE Command...OK
Testing: READ(10) Command...OK
Testing: MODE SENSE Command...OK
Testing: PREVENT-ALLOW MEDIUM REMOVAL Command...OK
Testing: REQUEST SENSE Command...OK
Testing: VERIFY Command...OK
Testing: WRITE(10) Command...OK
Testing: REQUEST SENSE Command...OK
Testing: START-STOP UNIT Command...OK

 

Ativa, No Model, 4GB, FAT32

=============START OF A NEW SESSION==================
VID = 0x05dc, PID = 0xa790
Testing: GET MAX LUN Command...OK
Testing: TEST UNIT READY Command...Unsupported by device (bStatus=0x97)
Testing: REQUEST SENSE Command...Unsupported by device (bStatus=0xfffffff9)
Testing: INQUIRY Command...Unsupported by device (bStatus=0xfffffff9)
Testing: REQUEST SENSE Command...Unsupported by device (bStatus=0xfffffff9)
Testing: READ FORMAT CAPACITIES Command...Unsupported by device (bStatus=0xfffffff9)
Testing: REQUEST SENSE Command...Unsupported by device (bStatus=0xfffffff9)
Testing: READ CAPACITY Command...Unsupported by device (bStatus=0xfffffff9)
Testing: REQUEST SENSE Command...Unsupported by device (bStatus=0xfffffff9)
Testing: READ(10) Command...Unsupported by device (bStatus=0xfffffff9)
Testing: MODE SENSE Command...Unsupported by device (bStatus=0xfffffff9)
Testing: PREVENT-ALLOW MEDIUM REMOVAL Command...Unsupported by device (bStatus=0xfffffff9)
Testing: REQUEST SENSE Command...Unsupported by device (bStatus=0xfffffff9)
Testing: VERIFY Command...Unsupported by device (bStatus=0xfffffff9)
Testing: WRITE(10) Command...Unsupported by device (bStatus=0xfffffff9)
Testing: REQUEST SENSE Command...Unsupported by device (bStatus=0xfffffff9)
Testing: START-STOP UNIT Command...Unsupported by device (bStatus=0xfffffff9)

0 件の賞賛
返信

7,913件の閲覧回数
Cdn_aye
Senior Contributor I

We have had a great deal of grief over this problem as well. What we found is that the speed of the USB Flash Drive is the deciding factor. The software consistently fails on very fast drives and always works on slower drives. The definition of slow and fast is open, but fast for us was about 30% faster than the slower drives. We have tried several drives and the ones that work for us on our in-house board are from SanDisk, and are the cheap ones from Costco 4G, 4 for 17$ on a card.

 

What I believe is the problem is that the MQX scheduler interrupts and gets between the USB transfer at a byte level and the transfer fails on a missed response. We have seen similar issues with the i2c driver where the ACK was missed because of the RTOS scheduling interrupt. This was verified by the MQX people in the development team in Europe. This was more prevalent in MQX 3.7 than 3.8. I don't think we have seen the i2c timeout in 3.8 as yet.

 

This problem makes it very difficult to deliver a product to a customer base that will use their own flash drives at some point. The entire product can be seen as unreliable or faulty. 

0 件の賞賛
返信

7,913件の閲覧回数
dwillett
Contributor I

Grief is a good way to put it.  I haven't seen problems with the canned example applications that come with MQX, but in real applications where there is a lot going on, problems with the USB drives happen frequently.  So I, too, am suspicious it has something to do with other peripherals interrupting the system, context switching, etc. We stayed on 3.7, we had consistent problems on 3.8 reading files from a USB stick on startup.  We are using the 5125 board.  For us two things usually happen, either the USB stick stops working all together and we have to pull it out and re-insert it to get it to work again, or we will see a string of corrupted data in the files we are writing out.  We really need this fixed.

0 件の賞賛
返信

7,913件の閲覧回数
LANCO_M4
Contributor II

We are not only seeing some USB drives that fail, but a significant difference in speed when opening a file. A few of the USB drives that we tried open the file in 8-9 sec. Other take ~40-60 sec to open the same file. No clear relation to USB speed or density of the drive. 

0 件の賞賛
返信

7,913件の閲覧回数
tomaszk
Contributor II

KINGSTON DATATRAVELER G2 4GB

 

CW 7.2, MQX 3.6, M52259DEMO

 

 =============START OF A NEW SESSION==================
VID = 0x0951, PID = 0x1624
Testing: GET MAX LUN Command...OK
Testing: TEST UNIT READY Command...OK

Testing: REQUEST SENSE Command                      Test stops here!

 

0 件の賞賛
返信

7,913件の閲覧回数
JuroV
NXP Employee
NXP Employee

Dear all,

 

I strongly recommend you to use msd_commands from MQX version 3.5 as there is one important bug fixed.

If you report your USB disk findings, please include always application, MQX version, board and target used for testing.

 

Thank you.

0 件の賞賛
返信

7,913件の閲覧回数
cw_weldon
Contributor I

My USB stick does not have VID and PID. The only info it has is Production Revision Level 1100.  It is provided by a third party and we have tone of it to distribute to our customers.

 

Runing the test for my USB stick does not result anything in HyperTerminal. To verify my setup, I also ran it with Freescale Metal-Black USB stick which shows all commands are OK.  

0 件の賞賛
返信

7,913件の閲覧回数
nibble
Contributor II

Hi, 

Trascend 8GB works nicely

 

regards

nibble 

0 件の賞賛
返信

7,913件の閲覧回数
nibble
Contributor II

TDK 8GB - Not Working (Works on Windows and on Mac)

 

here is the log:

shell> Mass Storage Device Attached

 

 =============START OF A NEW SESSION==================

Testing: GET MAX LUN Command...OK

Testing: TEST UNIT READY Command...OK

Testing: REQUEST SENSE Command...Unsupported by device (bStatus=0xfffffff8)

Testing: INQUIRY Command...Unsupported by device (bStatus=0xfffffff9)

Testing: REQUEST SENSE Command...Unsupported by device (bStatus=0xfffffff9)

Testing: READ FORMAT CAPACITIES Command...Unsupported by device (bStatus=0xfffff

ff9)

Testing: REQUEST SENSE Command...Unsupported by device (bStatus=0xfffffff9)

Testing: READ CAPACITY Command...Unsupported by device (bStatus=0xfffffff9)

Testing: REQUEST SENSE Command...Unsupported by device (bStatus=0xfffffff9)

Testing: READ(10) Command...Unsupported by device (bStatus=0xfffffff9)

Testing: MODE SENSE Command...Unsupported by device (bStatus=0xfffffff9)

Testing: PREVENT-ALLOW MEDIUM REMOVAL Command...Unsupported by device (bStatus=0

xfffffff9)

Testing: REQUEST SENSE Command...Unsupported by device (bStatus=0xfffffff9)

Testing: VERIFY Command...Unsupported by device (bStatus=0xfffffff9)

Testing: WRITE(10) Command...Unsupported by device (bStatus=0xfffffff9)

Testing: REQUEST SENSE Command...Unsupported by device (bStatus=0xfffffff9)

Testing: START-STOP UNIT Command...Unsupported by device (bStatus=0xfffffff9)

 

Test done! 

0 件の賞賛
返信

7,913件の閲覧回数
nibble
Contributor II

Some more devices:

- EutronSec Picodisk 512MB - OK

- SANDISK Cruzer U3 16GB (after uninstalling the U3 garbage and repartitioning it with only one partition) - Fails with the message:

 

************************************************************************
Vendor Information:     SanDisk  Mass Storage Device
Product Identification: U3 Cruzer Micro
Product Revision Level: 8.02
************************************************************************
Error while opening partition (UNKNOWN ERROR !!!)
Device removed, starting device cleanup
--->Closing MFS
--->Uninstalling
--->Uninstalling PM
--->Closing disk
--->Closing USB MFS 

 

The MSD_commands example returns the log:

 

 =============START OF A NEW SESSION==================
Testing: GET MAX LUN Command...OK
Testing: TEST UNIT READY Command...OK
Testing: REQUEST SENSE Command...OK
Testing: INQUIRY Command...OK
Testing: REQUEST SENSE Command...OK
Testing: READ FORMAT CAPACITIES Command...OK
Testing: REQUEST SENSE Command...OK
Testing: READ CAPACITY Command...OK
Testing: REQUEST SENSE Command...OK
Testing: READ(10) Command...OK
Testing: MODE SENSE Command...OK
Testing: PREVENT-ALLOW MEDIUM REMOVAL Command...OK
Testing: REQUEST SENSE Command...OK
Testing: VERIFY Command...OK
Testing: WRITE(10) Command...Unsupported by device (bStatus=0x1)
Testing: REQUEST SENSE Command...Unsupported by device (bStatus=0xfffffff9)
Testing: START-STOP UNIT Command...Unsupported by device (bStatus=0xfffffff9)

Test done!

 

0 件の賞賛
返信

7,913件の閲覧回数
EAI
Contributor IV

Working:

   Ultra 256M

   Sandisk (various sizes tested)

0 件の賞賛
返信

7,913件の閲覧回数
gianxx
Contributor I

Tested:

 

LAVOD 512MB FAT16 (0x06): OK

 

HD 160GB FAT32 LBA (0x0c) with IDEtoUSB bridge/adapter, seems work... 

0 件の賞賛
返信