Two version of MQX

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Two version of MQX

1,160 次查看
danielchai
Senior Contributor I

Hi,

I have two version of MQX 3.8 and 4.0 installed, and now I try to compile a demo code based on MQX4.0. But it gives me error.

Is it because that I installed two version of MQX?

Thanks.

0 项奖励
回复
3 回复数

986 次查看
c0170
Senior Contributor III

Hello Daniel Chai,

could you describe it more in details.

Which error does it show? Share your console. Have you checked what are values of MQX_PATH and MQX_ROOT in System variables? What demo ? What is your IDE?

Please read this: How to post in the MQX section and get an answer!

Regards,

c0170

0 项奖励
回复

986 次查看
danielchai
Senior Contributor I

Hi Martin,

Thank you.

I uninstall the old version MQX.

Base on CW10.4 and MQX4.0.1, I wanted to try the demo secwebserver_twrk60n512 project.

But when I tried to compile it, it has problems.

Bug1.png

bug2.png

bug3.png

The user_config.h for MQX is

config1.png

config2.png

config3.png

Is there something wrong with my setting?

Thank you.

0 项奖励
回复

986 次查看
c0170
Senior Contributor III

Hello Daniel Chai,

what you have shared with us it's Problems tab, it does not help at all, the console is the right output which includes valuable information. What you have shared just implies that you either have wrong PATHS in system variables, one of the system library has not been built. Those are just from top of my head :smileywink:

What does the console say, first error? Just copy - paste it here. Can you check PATHS system variables for MQX_ROOT and MQX_PATH? Verify Resources -> Linker resources in Project properties.

Does any other demo or any example fail as well?

Regards,

c0170

0 项奖励
回复