The DHCP question in the MQX

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

The DHCP question in the MQX

1,430件の閲覧回数
小勇邹
Contributor II

My device is MK64FN1M0VMD12.The hardware is TWR-K64F120M. My compiler is IAR 7.2.

The MQX is Freescale_MQX_4_1_TWRK64F120M.

I write a tftps program.

When the function “ipcfg_bind_staticip (phy_addr,
&ip_data)” is used to bind the IP.

The tftps can work immediately after the program print   "\nTFTP Server is running."

But when the function “ipcfg_bind_dhcp_wait(phy_addr, 1,&ip_data)” is used to bind the IP .The tftps can not work immediately after the program
print   "\nTFTP Server isrunning." It costs about 6 seconds to run the tffps .

What is the reason?

The source code.

0 件の賞賛
返信
2 返答(返信)

992件の閲覧回数
danielchen
NXP TechSupport
NXP TechSupport

Hi Robin:

I think this is normal, when you use ipcfg_bind_dhcp_wait, system will poll dhcp packet , it needs some time


Have a great day,
Daniel

0 件の賞賛
返信

992件の閲覧回数
小勇邹
Contributor II

{          /*Normal user application*/

      /* Init RTCS */       _RTCSPCB_init = 4;       _RTCSPCB_grow = 2;       _RTCSPCB_max = 8;             _RTCSTASK_stacksize = 4500;             error = RTCS_create();       if (error != RTCS_OK)       {           printf("RTCS failed to initialize, error = 0x%X\n", error);           _task_block();       }

      _IP_forward = TRUE;

      /* Bind IP address for each interface */       for (i = 0; (i < n_devices) && (n_devices != 0); i++)/*n_devices=1*/       {/*get address*/           _enet_address           address;           uint32_t                 phy_addr;           #if RTCSCFG_ENABLE_IP4           IPCFG_IP_ADDRESS_DATA ip_data;           #endif           phy_addr = i;           ip_addr[i] = IPADDR(A,B,C+i,D);

          ENET_get_mac_address(phy_addr, ip_addr[i], address);                     /* Init ENET device */           error = ipcfg_init_device (phy_addr, address);           if (error != RTCS_OK)           {               printf("IPCFG: Device n.%d init failed. Error = 0x%X\n", i, error);               _task_set_error(MQX_OK);               n_devices--;               i--;               continue;           }

          #if RTCSCFG_ENABLE_IP4           ip_data.ip      = ip_addr[i];           ip_data.mask    = ENET_IPMASK;           ip_data.gateway = 0;

#if DEMOCFG_ENABLE_DHCP      error = ipcfg_bind_dhcp_wait(phy_addr, 1, &ip_data);/*Binds Ethernet device to network using DHCP protocol (blocking mode).*/      if (error != RTCS_OK)      {          printf("DHCP Error %08x! Use static IP\n", error);

      error = ipcfg_bind_staticip (phy_addr, &ip_data);       if (error != RTCS_OK)       {        printf("\nIPCFG: Failed to bind static IP address. Error = 0x%X", error);        _task_block();       }                 }     #else      /* Bind IPv4 address */      error = ipcfg_bind_staticip (phy_addr, &ip_data);/*Binds Ethernet device to network using constant (static) IPv4 address information*/      if (error != RTCS_OK)      {       printf("\nIPCFG: Failed to bind static IP address. Error = 0x%X", error);       _task_block();      }

#endif

          #endif                    /*indexes[i] = (char*) _mem_alloc_zero(sizeof("\\index_x.html"));           if (indexes[i] == NULL)           {               printf("\n Failed to allocate memory.");               _task_block();           }*/                  ipcfg_get_ip(phy_addr, &ip_data);        printf("IP Address      : %d.%d.%d.%d\n\n",IPBYTES(ip_data.ip));                       /*Update the  fnet_params*/     UpdateFnetParams(address,ip_data);            fapp_params_to_flash();           }       

     

#if DEMOCFG_TFTP_SERVER    {     error = TFTPSRV_init("TFTP server", 7, 1000);/*create tftps task*/     if (error) {}     else     {printf("\nTFTP Server is running."); }       } #endif   

   #if 0

      /* Install trivial file system. HTTP server pages are stored there. */       error = _io_tfs_install("tfs:", tfs_data);             /* Start HTTP server on each interface */       for (i = 0; i < n_servers; i++)       {           _mem_zero(&params[i], sizeof(HTTPSRV_PARAM_STRUCT));           params[i].af = HTTP_INET_AF;  //IPv4, IPv6 or from config.h

          #if RTCSCFG_ENABLE_IP6           /* Set interface number here. Zero is any. */           params[i].ipv6_scope_id = HTTP_SCOPE_ID;           #endif

          sprintf(indexes[i], "\\index.html");           params[i].root_dir = "tfs:";           params[i].index_page = indexes[i];           params[i].auth_table = auth_realms;           printf("Starting http server No.%d on IP", i);           /*           ** If there is only one server listen on any IP address           ** so address can change in runtime (DHCP etc.).           ** Otherwise we will use static IP for server.           */           if (HTTP_INET_AF & AF_INET)           {               #if RTCSCFG_ENABLE_IP4               if ((i == 0) && (n_servers == 1))               {                   params[i].ipv4_address.s_addr = INADDR_ANY;               }               else               {                   params[i].ipv4_address.s_addr = ip_addr[i];               }               /* Print active IPv4 address */               printf(" %d.%d.%d.%d", IPBYTES(ip_addr[i]));               #endif           }           if (HTTP_INET_AF & AF_INET6)           {               #if RTCSCFG_ENABLE_IP6               IPCFG6_GET_ADDR_DATA data;               char prn_addr6[RTCS_IP_ADDR_STR_SIZE];                             ipcfg6_get_addr(0, 0, &data);

              if(inet_ntop(AF_INET6, &(data.ip_addr), prn_addr6, sizeof(prn_addr6)))               {                   /* Print active IPv6 address */                   printf("%s %s", (HTTP_INET_AF & AF_INET) ? " and" : "", prn_addr6);               }               #endif           }           /*           ** Maximum default number of available sockets in RTCS is six.           ** Maximum of two are used for HTTP server as listening sockets (one for IPv4 and one for IPv6).           ** So we take two of sockets and use them for sessions.           */           params[i].max_ses = 2;           params[i].cgi_lnk_tbl = (HTTPSRV_CGI_LINK_STRUCT*) cgi_lnk_tbl;

          /* There are a lot of static data in CGIs so we have to set large enough stack for script handler */           params[i].script_stack = 3000;           server[i] = HTTPSRV_init(&params[i]);                     printf("...");           if (server[i] == (uint32_t) RTCS_ERROR)           {               printf("[FAIL]\n");           }           else           {               printf("[OK]\n");           }       }       /* HTTP server initialization is done so we can start shell */

   #endif          /*_task_create(0, SHELL_TASK, 0);*/       //_task_create(0, RS485_TASK, 0);       /*Normal user application*/   }

0 件の賞賛
返信