problem lwgpio isr M52233demo board

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

problem lwgpio isr M52233demo board

1,307 Views
caioreiajive
Contributor I

Hi everyone,

I’m having a problem setting the irq7 int on M52233demo board. It just doesn’t enter the callback function and curiously don’t open BSP_SW2 port !!

It doesn’t get to callback function and doesn’t get LWGPIO_VALUE_LOW value.

Here comes the odd thing.

When I comment the "lwgpio_set_functionality statement" it prints “..pin7 – low – sw2=pressed..” when button pressed, but dont enter callback.

However the most strange thing is that when I change the statement “status = lwgpio_init(&IntPort,BSP_SW1, LWGPIO_DIR_INPUT, LWGPIO_VALUE_NOCHANGE); from BSP_SW1 to BSP_SW2”  I get printf("Initialising GPIO as input failed.\n");  that is, it doesn’t open the SW2 port while it opens SW1 port !!

I’m lost.  Tried lots of variations of this code.

My user define since it has other projects closed for this test, contain defines set to SPI, ADC, TCP/IP, SNMP, TIMER. I’m not quite sure if it makes any difference for this test.

Any help would be great.

The code is as follows:

void IntCallback(void* data)
{
        lwgpio_int_clear_flag((LWGPIO_STRUCT_PTR)data);
        
        printf ("..interrup port entered..");

}

/*TASK*-------------------------------------------------------------------

*

* Task Name : main_task

* Comments  :

*

*END*----------------------------------------------------------------------*/

void main_task

   (

      uint_32 dummy

   )

{

        MQX_FILE_PTR mySpiFd;  //not used now

        LWGPIO_STRUCT IntPort;

        boolean status;

        uint_32 vector;

       

        status = lwgpio_init(&IntPort,BSP_SW1, LWGPIO_DIR_INPUT, LWGPIO_VALUE_NOCHANGE);

        lwgpio_set_functionality(&IntPort, LWGPIO_MUX_NQ7_GPIO);     //BSP_SW1_MUX_IRQ);//

        lwgpio_set_attribute(&IntPort, LWGPIO_ATTR_PULL_UP, LWGPIO_AVAL_ENABLE);

              

        if (status != TRUE) {

               printf("Initialising GPIO as input failed.\n");

               //_mqx_exit(-1);

        }else

               status = lwgpio_int_init(&IntPort, LWGPIO_INT_MODE_FALLING);

       

        if (status != TRUE) {

               printf("Initialising pin for interrupt failed.\n");

               //_mqx_exit(-1);

        }

       

        vector = lwgpio_int_get_vector(&IntPort);

        if (NULL == (_int_install_isr(vector, IntCallback, (void *) &IntPort) ) )

                       printf ("..error setting isr callback..");

        //_bsp_int_init(vector, 3, 0, TRUE); 

       

        lwgpio_int_clear_flag(&IntPort);

        lwgpio_int_enable(&IntPort, TRUE);

       

  

   while ( 1 ) {

          

           if ( LWGPIO_VALUE_LOW == lwgpio_get_raw(&IntPort) ) {

                  printf (" ..pin7 - low - sw2=pressed..");

           }

}

}

0 Kudos
Reply
2 Replies

1,063 Views
soledad
NXP Employee
NXP Employee

Hi caio reia,

Could you please try using the below code?

/**HEADER********************************************************************

*

* Copyright (c) 2008 Freescale Semiconductor;

* All Rights Reserved                      

*

***************************************************************************

*

* THIS SOFTWARE IS PROVIDED BY FREESCALE "AS IS" AND ANY EXPRESSED OR

* IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO, THE IMPLIED WARRANTIES

* OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR PURPOSE ARE DISCLAIMED. 

* IN NO EVENT SHALL FREESCALE OR ITS CONTRIBUTORS BE LIABLE FOR ANY DIRECT,

* INDIRECT, INCIDENTAL, SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES

* (INCLUDING, BUT NOT LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR

* SERVICES; LOSS OF USE, DATA, OR PROFITS; OR BUSINESS INTERRUPTION)

* HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY, WHETHER IN CONTRACT,

* STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING

* IN ANY WAY OUT OF THE USE OF THIS SOFTWARE, EVEN IF ADVISED OF

* THE POSSIBILITY OF SUCH DAMAGE.

*

**************************************************************************

*

* $FileName: lwgpio.c$

* $Version : 3.7.2.0$

* $Date    : Mar-8-2011$

*

* Comments:

*

*   This file contains the source for the lwgpio example program.

*

*END************************************************************************/

#include <mqx.h>

#include <bsp.h>

/* Function prototypes */

void main_task(uint_32);

void int_service_routine(void *);

const TASK_TEMPLATE_STRUCT  MQX_template_list[] =

{

    /* Task Index, Function, Stack, Priority,   Name,          Attributes, Param, Time Slice */

    { 1,          main_task,  1500,        8, "main", MQX_AUTO_START_TASK,     0,          0 },

    { 0 }

};

volatile uint_32 int_counter;

void int_service_routine(void *pin)

{

    int_counter++;

    lwgpio_int_clear_flag((LWGPIO_STRUCT_PTR) pin);

}

/*TASK*-----------------------------------------------------

*

* Task Name    : main_task

* Comments     :

* This task executes 3 steps

* 1) set BSP_LED1 on and off if BSP_LED1 available

* 2) configure BSP_BUTTON1 for interrupt if possible and wait

*    for 5 interrupt calls

* 3) Drives BSP_LED1 according read from BSP_BUTTON1 or

*    drives BSP_LED1 automatically if BSP_BUTTON1 not available

*END*-----------------------------------------------------*/

void main_task

   (

      uint_32 initial_data

   )

{

    /* Structures holding information about specific pin */

    LWGPIO_STRUCT led1, btn1;

#if defined BSP_LED1

/************************************************

Open BSP_LED1 as output, drive the output level.

************************************************/  

   /* open file containing pin1 set of pins/signals */

    if (!lwgpio_init(&led1, BSP_LED1, LWGPIO_DIR_OUTPUT, LWGPIO_VALUE_NOCHANGE))

    {

        printf("Initializing LED1 GPIO as output failed.\n");

        _mqx_exit(-1);

    }

    lwgpio_set_functionality(&led1, BSP_LED1_MUX_GPIO);

    /* write logical 1 to all signals in the file (fast) */

    lwgpio_set_value(&led1, LWGPIO_VALUE_HIGH);

    lwgpio_set_value(&led1, LWGPIO_VALUE_LOW);

#endif //BSP_LED1

#if defined BSP_BUTTON1

/************************************************

Open BSP_BTN1 as input, initialize interrupt on

it and set interrupt handler. Wait until five

calls of handler were called.

***********************************************/ 

    /* opening pins/signals for input */

    if (!lwgpio_init(&btn1, BSP_BUTTON1, LWGPIO_DIR_INPUT, LWGPIO_VALUE_NOCHANGE))

    {

        printf("Initializing button GPIO as input failed.\n");

        _mqx_exit(-1);

    }

#ifdef BSP_BUTTON1_MUX_IRQ

    /* Some peripherals require to setup MUX to IRQ functionality */

    lwgpio_set_functionality(&btn1, BSP_BUTTON1_MUX_IRQ);

#endif

    if (!lwgpio_int_init(&btn1, LWGPIO_INT_MODE_FALLING))

    {

        printf("Initializing button GPIO for interrupt failed.\n");

    }

    else

    {

        printf("Button configured for interrupt, waiting 5 interrupt callbacks.\n");

        /* install gpio interrupt service routine */

        _int_install_isr(lwgpio_int_get_vector(&btn1), int_service_routine, (void *) &btn1);

        _bsp_int_init(lwgpio_int_get_vector(&btn1), 3, 0, TRUE);

        lwgpio_int_enable(&btn1, TRUE);

        while (int_counter < 5)

        { /* Wait till 5 button pushes were made */ }

        lwgpio_int_enable(&btn1, FALSE);

    }

#endif //BSP_BUTTON1

#if defined BSP_BUTTON1

/************************************************

Open BSP_BTN1 as input and read value from it.

Note that in previous test, the pin was

configured as interrupt and that is why it must

be reconfigured as standard GPIO.

***********************************************/ 

    /* opening pins/signals for input */

    if (!lwgpio_init(&btn1, BSP_BUTTON1, LWGPIO_DIR_INPUT, LWGPIO_VALUE_NOCHANGE))

    {

        printf("Initializing button GPIO as input failed.\n");

        _mqx_exit(-1);

    }

    lwgpio_set_functionality(&btn1, BSP_LED1_MUX_GPIO);

    /* It is not easy to generalize switch: every board has its own switch names */

    printf("Use SWITCH on board to switch LED on or off\n");

    while (TRUE)

    {

        /* read pin/signal status to pin list */

        if (LWGPIO_VALUE_HIGH == lwgpio_get_value(&btn1))

        {

            printf("LED OFF.\n");

#if defined BSP_LED1

            /* clear pin to 0 (fast) */

            lwgpio_set_value(&led1, LWGPIO_VALUE_LOW);

#endif //BSP_LED1

        }

        else

        {

            printf("LED ON.\n");

#if defined BSP_LED1

            /* set pin to 1 (fast) */

            lwgpio_set_value(&led1, LWGPIO_VALUE_HIGH);

#endif //BSP_LED1

        }

   }

#elif defined BSP_LED1

/************************************************

In case board does not have BUTTONS,

Only blink with LED.

************************************************/   

    /* It is not easy to generalize LED: every board has its own LED names */

    printf("Going to blink with LED\n");

    while (TRUE)

    {

        /* write logical 0 to the pin */

        lwgpio_set_value(&led1, LWGPIO_VALUE_LOW);

        _time_delay(1000);

        /* write logical 1 to the pin */

        lwgpio_set_value(&led1, LWGPIO_VALUE_HIGH);

        _time_delay(1000);

    }

#else //BSP_LED1, BSP_BUTTON1

    printf("Cannot show demo, no BSP_LED1 nor BSP_BUTTON1 defined for board.");

#endif //BSP_LED1, BSP_BUTTON1

/* EOF */


Have a great day,
Sol

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

1,063 Views
caioreiajive
Contributor I

Hi Sol,

Thanks for your reply and your help.  It worked !!!

I find interesting noticing for the comunity that in the m52233demo.h file , it seems to have an error setting SW2/BUTTON2/MUX GPIO.

Its set to GPIO_PIN1 while it should be GPIO_PIN4 !!

When trying to set button2 port with GPIO_PIN1 it gets an error and with GPIO_PIN4 works fine.

/*

** GPIO board specifications

*/

#define BSP_LED1    (GPIO_PORT_TC | GPIO_PIN0)

#define BSP_LED2    (GPIO_PORT_TC | GPIO_PIN1)

#define BSP_LED3    (GPIO_PORT_TC | GPIO_PIN2)

#define BSP_LED4    (GPIO_PORT_TC | GPIO_PIN3)

#define BSP_SW1     (GPIO_PORT_NQ | GPIO_PIN7)

#define BSP_SW2     (GPIO_PORT_NQ | GPIO_PIN1)

#define BSP_LED1_MUX_GPIO (LWGPIO_MUX_TC0_GPIO)

#define BSP_LED2_MUX_GPIO (LWGPIO_MUX_TC1_GPIO)

#define BSP_LED3_MUX_GPIO (LWGPIO_MUX_TC2_GPIO)

#define BSP_LED4_MUX_GPIO (LWGPIO_MUX_TC3_GPIO)

#define BSP_SW1_MUX_GPIO  (LWGPIO_MUX_NQ7_GPIO)

#define BSP_SW2_MUX_GPIO  (LWGPIO_MUX_NQ1_GPIO)

/* definitions for user applications */

#define BSP_BUTTON1   BSP_SW1

#define BSP_BUTTON2   BSP_SW2

#define BSP_SW1_MUX_IRQ   (1)

#define BSP_SW2_MUX_IRQ   (1)

#define BSP_BUTTON1_MUX_GPIO  BSP_SW1_MUX_GPIO

#define BSP_BUTTON2_MUX_GPIO  BSP_SW2_MUX_GPIO

#define BSP_BUTTON1_MUX_IRQ   BSP_SW1_MUX_IRQ

#define BSP_BUTTON2_MUX_IRQ   BSP_SW2_MUX_IRQ

0 Kudos
Reply