Task Breakpoints

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Task Breakpoints

1,660件の閲覧回数
yossikorenberg
Contributor I

Hello

I work with CodeWarrior 10.4. /MQX 4.0.1. /MCF52259 ColdFire Microcontroller And cyclone max.

I'm building a small program with two Task.
I put breakpoints   at every Task .

When the program starts running it stops at the breakpoints at first task then at second task.

Only  one time. And then no more stops

Why?

0 件の賞賛
返信
2 返答(返信)

1,500件の閲覧回数
Monica
Senior Contributor III

Hello Yossi!

Please keep us posted on this, did you find the answer in the documentation?

Best regards,

Monica.

0 件の賞賛
返信

1,500件の閲覧回数
c0170
Senior Contributor III

Hello Yossi Korenberg,

please read How to post in the MQX section and get an answer!

Regards,

c0170

0 件の賞賛
返信