TWR-MCF5225X

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
2,207件の閲覧回数
MQXuser
Contributor III

I need to send emails from my 52259EVB and I see there is an example for the TWR-MCF5225X.

If the boards use the same microcontroller, why cant I use the same example for my 52259EVB?

 

 

Regards,

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 解決策
1,183件の閲覧回数
PetrM
Senior Contributor I

You can use telnet2ser_m52259evb.mcp and just replace the source files. That should be the simplest way to do it.

 

PetrM

 

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,184件の閲覧回数
PetrM
Senior Contributor I

You can use telnet2ser_m52259evb.mcp and just replace the source files. That should be the simplest way to do it.

 

PetrM

 

0 件の賞賛
返信