TWR-MCF5225X

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

TWR-MCF5225X

Jump to solution
2,236 Views
MQXuser
Contributor III

I need to send emails from my 52259EVB and I see there is an example for the TWR-MCF5225X.

If the boards use the same microcontroller, why cant I use the same example for my 52259EVB?

 

 

Regards,

Labels (1)
Tags (1)
0 Kudos
Reply
1 Solution
1,212 Views
PetrM
Senior Contributor I

You can use telnet2ser_m52259evb.mcp and just replace the source files. That should be the simplest way to do it.

 

PetrM

 

View solution in original post

0 Kudos
Reply
1 Reply
1,213 Views
PetrM
Senior Contributor I

You can use telnet2ser_m52259evb.mcp and just replace the source files. That should be the simplest way to do it.

 

PetrM

 

0 Kudos
Reply