TWR-K60N512 + IAR + MQX example

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

TWR-K60N512 + IAR + MQX example

Jump to solution
1,575 Views
sebasira
Senior Contributor I

Hello to you all!!

I'd like to get started with K60 MCU and MQX. I can't seem to find any code example for MQX and TWR-K60N512...I' using IAR v6.3

I've installed:

- MQX 3.8

- TWRK60N512QSDLAB.exe

Thanks!

Tags (3)
0 Kudos
Reply
1 Solution
1,334 Views
JuroV
NXP Employee
NXP Employee

Hello, the code examples are in mqx/examples, usb/device/examples, usb/host/examples, rtcs/examples, mfs/examples folders for MQX 3.8 installation.

View solution in original post

0 Kudos
Reply
2 Replies
1,335 Views
JuroV
NXP Employee
NXP Employee

Hello, the code examples are in mqx/examples, usb/device/examples, usb/host/examples, rtcs/examples, mfs/examples folders for MQX 3.8 installation.

0 Kudos
Reply
1,334 Views
sebasira
Senior Contributor I

Hi Juraj, thanks for your reply!

I've seen them, but I was use to have an IDE Workspace file that I will open with IAR... now I discover, the "Add Existing Project" option.

Thanks!!!

0 Kudos
Reply