Socket Accept abort behaviour problem

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Socket Accept abort behaviour problem

跳至解决方案
2,310 次查看
chrissolomon
Contributor III

Hi,

I am working on a product which uses the Telnet server code supplied with RTCS.

In the product the server needs to be started and stopped on demand.

During testing it was noticed that the server creates 2 sockets when started, but when the server is shut down only one socket is closed.

I have looked through the code and it seems that in the  SOCK_STREAM_accept function a new socket is created, then the task blocks waiting for a connection.

When the server is shut down, the task exit handler is called, which frees the first socket, but the second socket is left.

This process is repeated each time the server is started or stopped.

Is there any work-around you can suggest for this?

Thanks

Chris

标记 (3)
1 解答
2,010 次查看
chrissolomon
Contributor III

Ok, I've found a solution - I have modified tcp_clos.c - I've changed TCP_Close_TCB, adding the following to the end of that function:

/*

    * Close any sockets opened by accept

    */

   prev_req = NULL;

   req = tcp_cfg->OPENS;

   while( req != NULL )

   {

       if( ( req->TCB_PTR == tcb ) && ( ( ( SOCKET_STRUCT_PTR )req->SOCKET )->TCB_PTR == NULL ) ) {

           void * toBeFreed = req;

           SOCK_Free_sock_struct( ( SOCKET_STRUCT_PTR )req->SOCKET );

           // Just in case any thread is blocked waiting for this, send req complete.

           RTCSCMD_complete( req, RTCSERR_TCP_CONN_RLSD );

           // Remove the request from the open requests list

           if( prev_req != NULL ) {

               prev_req->NEXT = req->NEXT;

           }

           else {

               tcp_cfg->OPENS = req->NEXT;

           }

           // Move on to the next request

           req = req->NEXT;

           // Free the old request.

           _mem_free( toBeFreed );

       }

       else {

           prev_req = req;

           req = req->NEXT;

       }

   }

This looks for any Open Requests with the same TCB pointer in the request (the TCB of the listening socket), and where the socket has a NULL TCB pointer, and frees the socket.

This does not free any sockets that were spawned by the listening socket that have connected (the socket TCB wouldn't be NULL in that case).

在原帖中查看解决方案

2 回复数
2,010 次查看
larrydemuth
Contributor III

I came across this problem also a while back. I had a similar solution, but I think I like yours better. I didnt do this: RTCSCMD_complete( req, RTCSERR_TCP_CONN_RLSD ); I'm going to try it out. Thanks!

0 项奖励
回复
2,011 次查看
chrissolomon
Contributor III

Ok, I've found a solution - I have modified tcp_clos.c - I've changed TCP_Close_TCB, adding the following to the end of that function:

/*

    * Close any sockets opened by accept

    */

   prev_req = NULL;

   req = tcp_cfg->OPENS;

   while( req != NULL )

   {

       if( ( req->TCB_PTR == tcb ) && ( ( ( SOCKET_STRUCT_PTR )req->SOCKET )->TCB_PTR == NULL ) ) {

           void * toBeFreed = req;

           SOCK_Free_sock_struct( ( SOCKET_STRUCT_PTR )req->SOCKET );

           // Just in case any thread is blocked waiting for this, send req complete.

           RTCSCMD_complete( req, RTCSERR_TCP_CONN_RLSD );

           // Remove the request from the open requests list

           if( prev_req != NULL ) {

               prev_req->NEXT = req->NEXT;

           }

           else {

               tcp_cfg->OPENS = req->NEXT;

           }

           // Move on to the next request

           req = req->NEXT;

           // Free the old request.

           _mem_free( toBeFreed );

       }

       else {

           prev_req = req;

           req = req->NEXT;

       }

   }

This looks for any Open Requests with the same TCB pointer in the request (the TCB of the listening socket), and where the socket has a NULL TCB pointer, and frees the socket.

This does not free any sockets that were spawned by the listening socket that have connected (the socket TCB wouldn't be NULL in that case).