Simple RTC causing unhandled interrupt

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Simple RTC causing unhandled interrupt

跳至解决方案
1,922 次查看
LordMarkFRT
Contributor II

Hi everyody. I'm using MCF52259demokit and MQX 3.6. I'm fightint against the main task that after 2 or 3 hours of running (or debugging) launches an unhandled interrupt. The only peripheral I'm using is the RTC with 1Hz interrupt. So I think that RTC must be the cause of the issue.

 

I'm attaching the code for anyone who wants to try it, or take a look at it to see if there is something wrong. 

 

Regards,

Marco

0 项奖励
回复
1 解答
1,655 次查看
LordMarkFRT
Contributor II

SEEMS solved by porting it to MQX 3.7.

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,656 次查看
LordMarkFRT
Contributor II

SEEMS solved by porting it to MQX 3.7.

0 项奖励
回复