Simple RTC causing unhandled interrupt

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Simple RTC causing unhandled interrupt

ソリューションへジャンプ
1,890件の閲覧回数
LordMarkFRT
Contributor II

Hi everyody. I'm using MCF52259demokit and MQX 3.6. I'm fightint against the main task that after 2 or 3 hours of running (or debugging) launches an unhandled interrupt. The only peripheral I'm using is the RTC with 1Hz interrupt. So I think that RTC must be the cause of the issue.

 

I'm attaching the code for anyone who wants to try it, or take a look at it to see if there is something wrong. 

 

Regards,

Marco

0 件の賞賛
返信
1 解決策
1,623件の閲覧回数
LordMarkFRT
Contributor II

SEEMS solved by porting it to MQX 3.7.

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,624件の閲覧回数
LordMarkFRT
Contributor II

SEEMS solved by porting it to MQX 3.7.

0 件の賞賛
返信