Shell examples with terminal I/o instead of pemicro

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Shell examples with terminal I/o instead of pemicro

跳至解决方案
1,251 次查看
ronysha
Contributor II

I am using IAR. In order to use the terminal I/o of the tool instead of external terminal e.g.. pemicro I have to do some settings, which I did.

I am able to  force the printf and gets functions to use the terminal I/O (by commenting the #define printf of fio.h).

But shell.c printf and similar commands still try to access the uart. I think that the shell library has been prebuilt and includes its own version of fio.h. Even when I changed user_config.h and did the rebuilding of MQX didn't help.

How can I force them to approach the terminal I/o too?

Thanks

0 项奖励
回复
1 解答
896 次查看
ronysha
Contributor II

I sorted it out.

The shell has to be rebuilt with those changes to have any effect.

It is working fine now.

Thanks

在原帖中查看解决方案

0 项奖励
回复
1 回复
897 次查看
ronysha
Contributor II

I sorted it out.

The shell has to be rebuilt with those changes to have any effect.

It is working fine now.

Thanks

0 项奖励
回复