Shell examples with terminal I/o instead of pemicro

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Shell examples with terminal I/o instead of pemicro

Jump to solution
1,250 Views
ronysha
Contributor II

I am using IAR. In order to use the terminal I/o of the tool instead of external terminal e.g.. pemicro I have to do some settings, which I did.

I am able to  force the printf and gets functions to use the terminal I/O (by commenting the #define printf of fio.h).

But shell.c printf and similar commands still try to access the uart. I think that the shell library has been prebuilt and includes its own version of fio.h. Even when I changed user_config.h and did the rebuilding of MQX didn't help.

How can I force them to approach the terminal I/o too?

Thanks

0 Kudos
Reply
1 Solution
895 Views
ronysha
Contributor II

I sorted it out.

The shell has to be rebuilt with those changes to have any effect.

It is working fine now.

Thanks

View solution in original post

0 Kudos
Reply
1 Reply
896 Views
ronysha
Contributor II

I sorted it out.

The shell has to be rebuilt with those changes to have any effect.

It is working fine now.

Thanks

0 Kudos
Reply