SPI communication between two controller

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

SPI communication between two controller

1,931 次查看
dasar_pavanraju
Contributor I

Hi All,

Using 2 MM9z1_638 controller for SPI master and SPI slave.

In datasheet it mentioned as when it configured as Master---->Clock should be bus clock/2

                                               when it configured as Slave---->Clock should be bus clock/4

So i decided to keep bus clock /4;

I am using bus clock as 28Mhz.

am using SPI to ensure both controllers are running on same time.

Initially mater will send character 'R'.Slave will reply with 'R'.

Then both will start executing there code.

To verify sync,I enabled 500ms timer. Every 500ms tone counter will increment both sided.

For every one sec master will ask counter value of slave and also stores its count value.If both counter are same then both are in sync.

But problem is 

in master = 2,4,6,8,...

from  slave =0,0,2,4

Initially two bytes getting 0.

Then i decided to send some dummy data from slave to master whenever interrupt hits.In this condition am getting proper value.

also i checked both are running on same speed.

Please let me know the problem.

Thanks,

Pavan

标记 (2)
1 回复

1,636 次查看
danielmartynek
NXP TechSupport
NXP TechSupport

Hi Pavan,

Please see my comments here:

https://community.nxp.com/thread/491560 

Thanks,

Daniel