S32 Design Suite - Installation issues

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S32 Design Suite - Installation issues

ソリューションへジャンプ
2,103件の閲覧回数
stso
Contributor III

Hello,

I've got Problems installing the S32 Design Studio IDE.

If I run the installer as admin it collects all data needed for the Installation, but aborts directly after with the errormessage "multiple instances of the installer not allowed. Exiting". If I run the installer as a regular user I get asked for admin-rights at the product-activation. When I enter my product-ID another error comes up (online as well as offline activation, screenshot below).

s32_install_cut.png

OS: Win7 Enterprise 64-Bit (6.1 Build 7601)

System manufacturer: Lenovo

Model: 4484Y1X

CPU: Intel Core i5 2.4 GHz

RAM: 4096 MB

Thanks in advance for your help.

0 件の賞賛
返信
1 解決策
1,995件の閲覧回数
stso
Contributor III

Solved the Problem after looking at the install logs. Seems like the installer doesn't ask for admin-rights when it tries to install the unistaller.

Worked fine after logging in as admin on my machine.

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
1,996件の閲覧回数
stso
Contributor III

Solved the Problem after looking at the install logs. Seems like the installer doesn't ask for admin-rights when it tries to install the unistaller.

Worked fine after logging in as admin on my machine.

0 件の賞賛
返信
1,995件の閲覧回数
danielchen
NXP TechSupport
NXP TechSupport

Thanks for your sharing and good luck!

0 件の賞賛
返信