S32 Design Suite - Installation issues

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32 Design Suite - Installation issues

Jump to solution
2,122 Views
stso
Contributor III

Hello,

I've got Problems installing the S32 Design Studio IDE.

If I run the installer as admin it collects all data needed for the Installation, but aborts directly after with the errormessage "multiple instances of the installer not allowed. Exiting". If I run the installer as a regular user I get asked for admin-rights at the product-activation. When I enter my product-ID another error comes up (online as well as offline activation, screenshot below).

s32_install_cut.png

OS: Win7 Enterprise 64-Bit (6.1 Build 7601)

System manufacturer: Lenovo

Model: 4484Y1X

CPU: Intel Core i5 2.4 GHz

RAM: 4096 MB

Thanks in advance for your help.

0 Kudos
Reply
1 Solution
2,014 Views
stso
Contributor III

Solved the Problem after looking at the install logs. Seems like the installer doesn't ask for admin-rights when it tries to install the unistaller.

Worked fine after logging in as admin on my machine.

View solution in original post

0 Kudos
Reply
2 Replies
2,015 Views
stso
Contributor III

Solved the Problem after looking at the install logs. Seems like the installer doesn't ask for admin-rights when it tries to install the unistaller.

Worked fine after logging in as admin on my machine.

0 Kudos
Reply
2,014 Views
danielchen
NXP TechSupport
NXP TechSupport

Thanks for your sharing and good luck!

0 Kudos
Reply