Re: Using httpsrv to access web pages on SDcard

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Re: Using httpsrv to access web pages on SDcard

ソリューションへジャンプ
3,134件の閲覧回数
thom_nic
Contributor II

Reference to:

Using httpsrv to access web pages on SDcard

Is this demo source available somewhere?  I'm attempting to do something similar (serve files from flash/ SD.)  From your description I found a TWR-K60 quick start demo.zip however the archive only contains a .exe file (not helpful for folks on Mac/ Linux.)

Pointer to source material would be greatly appreciated - thanks!

1 解決策
2,978件の閲覧回数
soledad
NXP Employee
NXP Employee

Hello,

Attached to this thread, you can find the Quick Start Demo for the K60. In the thread you refer, the customer modified the code so unfortunately we don’t have exact code you need.


Have a great day,
Sol

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

4 返答(返信)
2,979件の閲覧回数
soledad
NXP Employee
NXP Employee

Hello,

Attached to this thread, you can find the Quick Start Demo for the K60. In the thread you refer, the customer modified the code so unfortunately we don’t have exact code you need.


Have a great day,
Sol

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

2,978件の閲覧回数
thom_nic
Contributor II

Of course, this is all I was looking for.  Thanks for posting the demo!

0 件の賞賛
返信
2,978件の閲覧回数
RadekS
NXP Employee
NXP Employee

BTW: alias for access to MFS file system is used also in web_hwac demo code (in this case it is USB flash disk). Example of path to this demo:

c:\Freescale\Freescale_MQX_4_2\demo\web_hvac

Please look at rtcs.c file.

I hope it helps you.

Have a great day,
RadekS

2,978件の閲覧回数
thom_nic
Contributor II

Hey RadekS, thanks that's very helpful.  I wouldn't have guessed!

0 件の賞賛
返信