RTCS with HTTP server tasks with time slice

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

RTCS with HTTP server tasks with time slice

1,667件の閲覧回数
nicolasguigo
Contributor II

Hello,

We have a project running with the following environment: KDS (1.3.0) with KSDK (3.0.0) and Processor Expert (PEX). We did a small web server with a few HTML pages. I believe that when the pages are display, the RTCS task and/or the HTTP server take a very long time to reply to the requests.

Observation 1: The watchdog not being kicked during more than a second

On our board, we have a hardware watchdog which is set to a little more than 1 second. The function kicking the watchdog is in the main task which have the highest priority and do nothing more than kicking the watchdog every 100ms.

By tracking the watchdog kicks, we can observe that, when a page is requested, the watchdog is not kicked at the same frequency it normally is. Hitting the "F5" key in the browser to generate multiple requests may even make our system reboot (because the watchdog has not been kicked during more than a second).

Observation 2: The UART communication being held up during more than 250ms

In our full system, there are 2 microcontrollers, they communicate using UART. There is a 250ms timer which is refreshed every time a word is received from the other microcontroller. When the web pages are not accessed, there are no issues (the system has been on for days). When the pages are displayed (even a few seconds after booting up), it may happen that the timer expires.

Note : Not to have a task holding up the processing time, we created the tasks with the option MQX_TIME_SLICE_TASK.

I believe creating the RTCS related tasks with the MQX_TIME_SLICE_TASK option may be a solution to the encountered problem. So I guess my question is: how to make the RTCS related tasks share their running time on a time slice base? As I stated before, it may not be the solution so I'm also open to suggestions/ideas on what to do to solve this problem.

ラベル(1)
タグ(5)
0 件の賞賛
返信
1 返信

1,521件の閲覧回数
danielchen
NXP TechSupport
NXP TechSupport

Hi Nicolas:

Have you fixed this issue?

I noticed there is one issue in MQX 4.2.0 (the rtcs stack is the same as that in KSDK1.3), might be involved with the MQX bug: MQX-5609.

pastedImage_1.png

If this is the case, there is a patch to fix this, MQX 4.2.0.2.

Regards

Daniel

0 件の賞賛
返信