RTCS performance

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
7,357件の閲覧回数
admin
Specialist II

I have ported NETIO TCPIP server to measure network performance of RTCS. The test sends 1k, 2k, 4k, 8k, and 16k data blocks and measures the data thought based on the time around. The test was done for MFC52259 evb. Here are the results:

 

Packet size, Bytes   RX speed, Bytes/s     TX Speed Bytes/s
1024                          114688                           6627

2048                          139264                           22071

4096                          212992                          18542

8192                          305152                          19156

16384                        424960                          240640

 

It seems the transmission speed is really low. Do you have any similar test results showing different performance or this is the actual performance we have to expect? 

 

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 解決策
4,175件の閲覧回数
admin
Specialist II

NETIO original source code and Windows binary could be found on:

http://www.ars.de/ars/ars.nsf/docs/netio

Dmitri.

元の投稿で解決策を見る

0 件の賞賛
返信
4 返答(返信)
4,175件の閲覧回数
EAI
Contributor IV

The default build parameters for RTCS for the 52259 are set to optimize memory, not speed. There are a number of parameters that can be adjusted that will result in better throughput, at the expense of additional memory. If you want to provide your NETIO port, we may be able to suggest which parameters should change.

0 件の賞賛
返信
4,175件の閲覧回数
admin
Specialist II

I have been using minimal RAM configuration which is default for MFC52259 and tried to change the socket options for buffer sizes (OPT_TBSIZE, OPT_RBSIZE) improve performance. Nothing worked. I have attached the port to the message.

 

MFC52259_netio.zip

Message Edited by t.dowe on 2009-09-22 12:42 PM
0 件の賞賛
返信
4,174件の閲覧回数
EAI
Contributor IV
Thanks. There are other parameters that will also affect performance. Will update you after looking at the code.
0 件の賞賛
返信
4,176件の閲覧回数
admin
Specialist II

NETIO original source code and Windows binary could be found on:

http://www.ars.de/ars/ars.nsf/docs/netio

Dmitri.

0 件の賞賛
返信