RTCS failed to initialize, error = 1136

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

RTCS failed to initialize, error = 1136

ソリューションへジャンプ
2,429件の閲覧回数
pmt
Contributor V

I've changed my reference BSP configuration to disable RTCS_MINIMUM_FOOTPRINT, as I need support for multicast.  Unfortunately when I do this RTCS fails to initialize at run-time with error 1136 (I'm using MQX 4.0.1).   

The RTCS startup is somewhat convoluted so it's not easy to debug/troubleshoot but I gathered that this is an RTCSERR_OPEN_QUEUE_FAILED when calling RTCS_task_create().  Is there some run-time dependency I need to change?  I am running the "small_ram_config" defaults. 

Thanks,

PMT

ラベル(1)
タグ(3)
0 件の賞賛
返信
1 解決策
2,209件の閲覧回数
butok
NXP Employee
NXP Employee

Please do not change the RTCS_MINIMUM_FOOTPRINT parameter (it is more for internal usage 0=MPUs, 1=MCUs).

If you need to enable a feature that is disabled, just use a configuration option that corresponds to it.

BTW:

     In 4.1.0 the RTCS_MINIMUM_FOOTPRINT will  disappear, to avoid this type of wrong settings.

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
2,210件の閲覧回数
butok
NXP Employee
NXP Employee

Please do not change the RTCS_MINIMUM_FOOTPRINT parameter (it is more for internal usage 0=MPUs, 1=MCUs).

If you need to enable a feature that is disabled, just use a configuration option that corresponds to it.

BTW:

     In 4.1.0 the RTCS_MINIMUM_FOOTPRINT will  disappear, to avoid this type of wrong settings.

0 件の賞賛
返信
2,209件の閲覧回数
pmt
Contributor V

Andrey,

Good info.  In user.config.h I re-enabled RTCS_MINIMUM_FOOTPRINT and added RTCSCFG_ENABLE_IGMP, and this seemed to take care of the issue.

My board is a derivation from the original K60 tower BSP with lots more memory.  Are you saying even then I should leave RTCS_MINIMUM_FOOTPRINT enabled, and simply pick the services I need?

Thanks,

PMT

0 件の賞賛
返信
2,209件の閲覧回数
butok
NXP Employee
NXP Employee

"RTCS_MINIMUM_FOOTPRINT" is "mistake of nature".

>>Are you saying even then I should leave RTCS_MINIMUM_FOOTPRINT enabled, and simply pick the services I need?

Yes.

0 件の賞賛
返信