RTCS Webserver

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

RTCS Webserver

2,480 Views
monakhanafriboo
Contributor II

I have trouble finding the IP address for the Freescale RTCS Webserver? I had 192.168.1.202 and was working but now its not, I couldnt reach the server with this IP address any idea if that IP been changed ?

i used to get this page with this ip : rtcs_freescle.jpg

Labels (1)
0 Kudos
Reply
3 Replies

2,257 Views
pbanta
Contributor IV

Did you configure that static IP address or was it assigned to your board by a DHCP server?  What version of MQX are you using?

0 Kudos
Reply

2,257 Views
monakhanafriboo
Contributor II

Hi phanta,

Thank you for your reply

this is a Demo example that in kdk1.2

C:\Freescale\KSDK_1.2.0\middleware\tcpip\rtcs\examples\httpsrv\build\kds\httpsrv_frdmk64f

but my concerns not about the demo itself, it's about the ip address, when I put 192.168.1.202 in my browser should bring that "webserver" page to make sure its reachable before running the demo.

0 Kudos
Reply

2,257 Views
soledad
NXP Employee
NXP Employee

Hello,

It is possible something is corrupted in the demo code. Attached you can find the project folder, copy it into the example folder and test again.

Please let me know if this helps!


Have a great day,
Sol

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply