Project creation for FRDMK66F

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Project creation for FRDMK66F

1,532件の閲覧回数
unnikrishnanm
Contributor I

I want to create a project with the following :

Board - FRDMK66F

RTOS - MQX

Interfaces - UART, SPI, I2C, SDIO

Additional features - RTCS, USB, LWIP

Toolchain - KDS

Please help me to do this. It will be very helpful, if you can share the document which contains the procedure followed.

0 件の賞賛
返信
1 返信

1,176件の閲覧回数
danielchen
NXP TechSupport
NXP TechSupport

Hi UNNIKRISHNAN M

I would like to suggest you read the following document for creating a MQX project with KDS.

How To: Create a New MQX RTOS for KSDK Project in KDS 

If you use IAR, please refer to the following link

https://community.nxp.com/docs/DOC-105525 

You also can refer to the MQX demo project based on K66 in ksdk.

C:\Freescale\KSDK_1.3.0\examples\frdmk66f\demo_apps\i2c_rtos\i2c_rtos_mqx\kds


Have a great day,
Daniel

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信