Problems with D4D library

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Problems with D4D library

2,065件の閲覧回数
alejandraartal
Contributor I

Hi, I have been trying to compile a projecto with the D4D Library. I'm using CodeWarrior 10.7, MQX 4.0 and the module k40x256. I'm new on that, but I have done the steps given by the AN4644 guide. I solved many of the compilation errors, but it's still producing more of them, the majority comming from D4D documents. So, I'm here asking for any help . I attached my project and some pictures. I wonder if someone could try to compile it, to verify that it is not my system.

Note: I have tried to compile the project with MQX 4.1 and 4.2, but I got no better results. Thank you in advance.

0 件の賞賛
返信
1 返信

1,777件の閲覧回数
danielchen
NXP TechSupport
NXP TechSupport

Hi  Alejandra

The original file was tested with MQX 4.0.0 and CW 10.3.

I would suggest you take a look at below thread , you can download the package build with MQX 4.0.2 / CW 10.5  , and with MQX 4.1 / CW10.6,  Please refer to below link for more details

TWR-K70F120M + TWR-LCD-RGB using CodeWarrior + eGUI code example 

Regards

Daniel

0 件の賞賛
返信