Problem: Installing MQX RTOS Task Aware Debugger for GDB plug-in (TAD)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Problem: Installing MQX RTOS Task Aware Debugger for GDB plug-in (TAD)

Jump to solution
9,754 Views
jeffreygraves
Contributor III

Just installed KDS 2.0.0.

Following steps in "Getting Started with Freescale MQX RTOS for Kinetis SDK and Kinetis Design Studio IDE", Doc No: KSDKGSKDSUG.

Sec 2.1: Installing MQX RTOS Task Aware Debugger for GDB plug-in (TAD)

Try to access:

Freescale KDS Update Site - http://freescale.com/lgfiles/updates/Eclipse/KDS

Get error:

Unable to read repository at http://freescale.com/lgfiles/updates/Eclipse/KDS/content.jar

I have verified that this still works with KDS 1.1.0.

Does anyone have a work around for this?

Thanks,

Tags (3)
0 Kudos
Reply
1 Solution
8,068 Views
jeffreygraves
Contributor III

From my home network I am able to access the update site via KDS_2.0.0 just fine.

View solution in original post

0 Kudos
Reply
7 Replies
8,069 Views
jeffreygraves
Contributor III

From my home network I am able to access the update site via KDS_2.0.0 just fine.

0 Kudos
Reply
8,068 Views
DavidS
NXP Employee
NXP Employee

Hi Jeffrey,

Ok...good to know.  Seems like IT has struck again!

Regards,

David

0 Kudos
Reply
8,068 Views
DavidS
NXP Employee
NXP Employee

Hi Jeffrey,

I was able to access the update using KDS2.0.0.

But I had to only select the TAD update by itself to get it to install.

I then did re-start and re-peated the process for the Project in Project update to allow importing Working Sets.

Regards,

David

8,068 Views
jeffreygraves
Contributor III

Which platform are you on?

I am not able to access the update with KDS 2.0.0 (W7x86 or W7x64).

I can access the update with KDS 1.1.1.

I will try this again later from home and off of our corporate network.

Any other ideas?

Thank you for your update.

Best regards,

0 Kudos
Reply
8,063 Views
DavidS
NXP Employee
NXP Employee

Hi Jeffrey,

I’m on W7x64.

I am assuming you updated the Eclipse first by pointing to the KSDK following path?

C:\Freescale\KSDK_1.1.0\tools\eclipse_update

The picture of my “Available Software” updates is:

NOTE: I only check on box, to the update. Restart the IDE, then do the other box. Then restart again.

Regards,

David

0 Kudos
Reply
8,063 Views
jeffreygraves
Contributor III

David,

I did update eclipse as you describe.  I did not get the picture of your available software updates.

From KDS_2.0.0, I keep getting the provisioning error:

Unable to read repository at http://freescale.com/lgfiles/updates/Eclipse/KDS/content.jar.

This is an ongoing problem...

I was able to install "MQX Task Aware Debugger for GDB" by making a local mirror of:

http://freescale.com/lgfiles/updates/Eclipse/KDS

I had to use my PExDrv v10.4 eclipse install to make the local mirror copy.

**My KDS_2.0.0 exlipse install could still not get at the update site.

(I could email you an error log...)

I followed these steps to generate the command lines that got me the local mirror:

http://mcuoneclipse.com/2014/07/03/replicating-an-eclipse-update-site-for-offline-usage/

Once I got a local mirror of the updates, I was able to update KDS_2.0.0 with "MQX Task Aware Debugger for GDB".

I found a painful workaround, but not a fix...

Best regards,

8,063 Views
barrymcnamara
Contributor II

Can confirm--I was only able to install after creating a mirror of the repo.

I found this guide very helpful: https://mcuoneclipse.com/2014/07/03/replicating-an-eclipse-update-site-for-offline-usage/

0 Kudos
Reply