It means no route to host.
Its because Freescale hasn't fixed their PPP driver (which also has infinate loops in it as well - so some of your RTCS functions will lock up your code when the ppp link is down).
This is what I did to fix the issue:
static boolean IPCP_up ( PPPFSM_CFG_PTR fsm /* [IN] - State Machine */ ){ /* Body */ IP_IF_PTR if_ptr = fsm->PRIVATE; IPCP_CFG_STRUCT_PTR ipcp_ptr = if_ptr->HANDLE; /* Bind the negotiated IP address to this interface */ ipcp_ptr->BIND_PARMS.ihandle = if_ptr; ipcp_ptr->BIND_PARMS.address = ipcp_ptr->LOPT.ADDR; ipcp_ptr->BIND_PARMS.network = ipcp_ptr->POPT.ADDR?ipcp_ptr->POPT.ADDR:((ipcp_ptr->LOPT.ADDR & IN_CLASSC_NET) + 1); //ipcp_ptr->BIND_PARMS.network = ipcp_ptr->POPT.ADDR; ipcp_ptr->BIND_PARMS.netmask = INADDR_ANY; RTCSCMD_smartissue(ipcp_ptr->BIND_PARMS, IPIF_bind_ppp); /* Install a default gateway */ if (ipcp_ptr->INIT.DEFAULT_ROUTE) { ipcp_ptr->GATE_PARMS.address = ipcp_ptr->POPT.ADDR?ipcp_ptr->POPT.ADDR:((ipcp_ptr->LOPT.ADDR & IN_CLASSC_NET) + 1); //ipcp_ptr->GATE_PARMS.address = ipcp_ptr->POPT.ADDR; ipcp_ptr->GATE_PARMS.network = INADDR_ANY; ipcp_ptr->GATE_PARMS.netmask = INADDR_ANY; /* Start CR 1133 */ ipcp_ptr->GATE_PARMS.locmask = 0; /* End CR 1133 */ RTCSCMD_smartissue(ipcp_ptr->GATE_PARMS, IPIF_gate_add); } /* Endif */#if RTCSCFG_ENABLE_DNS || RTCSCFG_ENABLE_LWDNS /* Set up the primary DNS server */ if (ipcp_ptr->NEG.NEG_DNS) {#if RTCSCFG_ENABLE_DNS /* Start CR 2257 */ DNS_SLIST_STRUCT slist_entry; DNS_init_slist_entry(&slist_entry); slist_entry.IPADDR = ipcp_ptr->LOPT.DNS; if (DNS_add_slist_entry(&slist_entry) != DNS_OK) return FALSE; /* End CR 2257 */#else LWDNS_server_ipaddr = ipcp_ptr->LOPT.DNS;#endif } /* Endif */#endif if (ipcp_ptr->IP_UP) { ipcp_ptr->IP_UP(ipcp_ptr->IP_PARAM); } /* Endif */ return TRUE;} /* Endbody */