Out of memory

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Out of memory

1,119 Views
antonsvensson
Contributor I

Hello.

I've run out of RAM in my application.

I'm running an k20...120 which should have a RAM capacity of 128k (0x1fff0000 - 0x2000fff0)

I've based my BSP on the TWRK60M120 BSP.

What I can see when running my application and checking the lwmemory pool is based from 0x1fff8330 - 0x2000fff0 which is about 95k ram.

Does anyone know where this RAM goes?

Best regards

Tags (3)
0 Kudos
Reply
1 Reply

965 Views
soledad
NXP Employee
NXP Employee

Hi Anton,

Could you please check the below thread?, Please let me know if this helps :smileywink:

MQX memory usage
Have a great day,
Sol

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply