Out of memory

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Out of memory

1,097 次查看
antonsvensson
Contributor I

Hello.

I've run out of RAM in my application.

I'm running an k20...120 which should have a RAM capacity of 128k (0x1fff0000 - 0x2000fff0)

I've based my BSP on the TWRK60M120 BSP.

What I can see when running my application and checking the lwmemory pool is based from 0x1fff8330 - 0x2000fff0 which is about 95k ram.

Does anyone know where this RAM goes?

Best regards

标记 (3)
0 项奖励
回复
1 回复

943 次查看
soledad
NXP Employee
NXP Employee

Hi Anton,

Could you please check the below thread?, Please let me know if this helps :smileywink:

MQX memory usage
Have a great day,
Sol

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复