The bootloader is programmed from 0x0~0x9FFF.
Application is programmed begin from 0xA000.
After bootloader programming the application, it will jump to 0xA000.
So, we need to modify the MQX application project to begin from 0xA000.
We've modify below settings.
#define BSP_INTERNAL_FLASH_BASE 0x0000A000
#define __VECTOR_TABLE_ROM_START 0x0000A000
#define MQX_ROM_VECTORS 0
We also modify the .scf file with below value, original is 0x00000000.
| #define INTFLASH_BASE_ADDR | 0x0000A000 |
The map file seems ok, but can not execute the application correctly.
| .vectors_rom | 0x0000a000 Section | 1024 vectors.o(.vectors_rom) |
| __tagsym$$used | 0x0000a000 Number | 0 vectors.o(.vectors_rom) |
| .cfmconfig | 0x0000a400 Section | 16 vectors.o(.cfmconfig) |
| __tagsym$$used | 0x0000a400 Number | 0 vectors.o(.cfmconfig) |
| !!!main | 0x0000a410 Section | 8 __main.o(!!!main) |
| !!!scatter | 0x0000a418 Section | 52 __scatter.o(!!!scatter) |
| !!dczerorl2 | 0x0000a44c Section | 90 __dczerorl2.o(!!dczerorl2) |
| !!handler_copy | 0x0000a4a8 Section | 26 __scatter_copy.o(!!handler_copy) |
| !!handler_zi | 0x0000a4c4 Section | 28 __scatter_zi.o(!!handler_zi) |
| . text | 0x0000a4e0 Section | 76 boot.o(. text) |
Did we miss some configuration so it can not be executed correctly ?
Please advise, thanks.