Bind more than one OID to trap v1

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Bind more than one OID to trap v1

1,031件の閲覧回数
davidboutet
Contributor I

Hi,

I would like to bind more than one SNMP object to SNMPv1 trap.

The example shows:

SNMP_trap_userSpec( (RTCS_NODE *)&MIBNODE_counter, TRAP_SPC, (RTCSMIB_NODE *)&MIBNODE_your_company );

I can only attach one MIB node ("MIB_NODE_counter" in the example). How to attach a list instead?


ラベル(1)
タグ(3)
0 件の賞賛
返信
2 返答(返信)

922件の閲覧回数
soledad
NXP Employee
NXP Employee

Hi David,

Could you please provide  a little more information?

Are you using  a Freescale board?

Are you using MQX?

Have a great day,
Sol

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

922件の閲覧回数
davidboutet
Contributor I

I'm using MQX4.1, CW10.5 and my own custom board containing K60DN512VLL10 chip.

0 件の賞賛
返信