MQX usb Device stack Vbus ISR Configuration

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MQX usb Device stack Vbus ISR Configuration

1,022 Views
panks
Contributor I

Hi,

I have used the mqx usb device stack for my usb application. I have used IRQ6 pin interrupt to detect vbus attached event , with the help of mqx gpio example code of mcf54418 stack.

My question is that,

When I am plugging In usb connector, the interrupt comes and control goes to ISR function but it continuously cal ISR after i have removed usb connector. I have set  EPFR resigister bit in ISR using till no effect.

Where should i am wrong? Which register I have to configure in ISR so that ISR cal only one time.

Regards,

Panks

Labels (1)
0 Kudos
Reply
0 Replies