MQX tasks of 1 ms repeat every 10 ms

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MQX tasks of 1 ms repeat every 10 ms

Jump to solution
1,080 Views
ZeusEscudero
Contributor I

Dear Community, we are using MQX in a Kinetis K60. We need task with repetitions every 100 ms, 10 ms and 1 ms.

Tasks of 100  and 10 ms work well but the task for repetition every 1 ms repeats actually every 10 ms.

That is the limit of the OS or there is a switch to configure to get tasks every 1 ms?

Thank you in advance for your help

Sincerely

Zeus

0 Kudos
Reply
1 Solution
833 Views
c0170
Senior Contributor III

Hi Zeus Escudero,

 

is set in BSP. Check BSP_ALARM_FREQUENCY in twrk60n512.h file. Description is in the MQX User Guide.

 

Regards,

MartinK

 

 

View solution in original post

0 Kudos
Reply
1 Reply
834 Views
c0170
Senior Contributor III

Hi Zeus Escudero,

 

is set in BSP. Check BSP_ALARM_FREQUENCY in twrk60n512.h file. Description is in the MQX User Guide.

 

Regards,

MartinK

 

 

0 Kudos
Reply