CPU, CORE and BUS frequencies, FNET configuration and MQX configuration

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

CPU, CORE and BUS frequencies, FNET configuration and MQX configuration

跳至解决方案
1,034 次查看
Skyhawk
Contributor I

Hi all,

 

I'm working on the TWR-K60N512 tower, in the gettings started pdf, I read about the TWR-K60N512 board.

 

Core Clock 96 MHz
Bus Clock 48 MHz

 

However on both the TWR-K60N512 board and the TWR-SER board there are 50Mhz oscilators.

How do the external oscillator frequecies correspond to the Core and Bus frequencies?

 

Greetings,


 

 

0 项奖励
回复
1 解答
847 次查看
c0170
Senior Contributor III

Hi Skyhawk,

 

Please check this document : K60 Reference Manual chapter 5 Clock distribution. There are located clocking diagram, clock definitions and internal clock requirements.

 

Regards,

MartinK

在原帖中查看解决方案

0 项奖励
回复
1 回复
848 次查看
c0170
Senior Contributor III

Hi Skyhawk,

 

Please check this document : K60 Reference Manual chapter 5 Clock distribution. There are located clocking diagram, clock definitions and internal clock requirements.

 

Regards,

MartinK

0 项奖励
回复