MQX support for Vybrid QSPI1

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MQX support for Vybrid QSPI1

ソリューションへジャンプ
1,091件の閲覧回数
nancyb
Contributor III

When will MQX support QSPI1 on Vybrid? Are there issues that prevent cloning the QSPI0 support to support QSPI1?

Regards,

Nancy

0 件の賞賛
返信
1 解決策
931件の閲覧回数
nancyb
Contributor III

Hi RadekS,


I found the problem:we use a tailored MQX 4.1 and QSPI1 was edited out. When I looked at my local MQX 4.1 installation I see the missing support.

Now to add it back to our official version.

Thank you for your help.

Regards,

Nancy

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
931件の閲覧回数
RadekS
NXP Employee
NXP Employee

Hi Nancy,

there should not be any issue with QSPI1.

QSPI driver include low level driver supports QSPI1.

twrvf65gs10 contains two Flash chips connected to QSPI0_A and QSPI0_B.

vybrid_autoevb contains three Flash chips connected to QSPI0_A, QSPI0_B and QSPI1.

Do you know about any specific issue with QSPI1?


Have a great day,
RadekS

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信
932件の閲覧回数
nancyb
Contributor III

Hi RadekS,


I found the problem:we use a tailored MQX 4.1 and QSPI1 was edited out. When I looked at my local MQX 4.1 installation I see the missing support.

Now to add it back to our official version.

Thank you for your help.

Regards,

Nancy

0 件の賞賛
返信
931件の閲覧回数
RadekS
NXP Employee
NXP Employee

Thank you for your clarification.

Now it make sense.

0 件の賞賛
返信