Bug Report: Security problem in HTTP Server

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Bug Report: Security problem in HTTP Server

1,160件の閲覧回数
chrissolomon
Contributor III

Hi,

I am just looking at the changes in MQX 4.1.0, and I happened to notice a minor bug in the HTTP server.

I don't think this will break anything, but it looks like the behavior is not as intended.

This is from httpsrv_task.c, line 824:

static void httpsrv_ses_free(HTTPSRV_SESSION_STRUCT *session)

{

    if (session)

    {

        if (session->request.path)

        {

            _mem_free(session->request.path);

        }

        if(session->request.auth.user_id)

        {

            _mem_free(session->request.auth.user_id);

        }

        if(session->buffer.data)

        {

            _mem_free(session->buffer.data);

        }

        _mem_zero(session, sizeof(session));

        _mem_free(session);

    }

}

It looks like the intention is to zero out the HTTPSRV_SESSION_STRUCT before freeing it, but using sizeof(session) is only going to zero the size of a pointer.

Since you are going to the trouble of zeroing the session structure immediately before freeing it the session struct must contain information that you consider sensitive, so this is probably a security problem.

Chris

ラベル(1)
タグ(3)
0 件の賞賛
返信
1 返信

1,032件の閲覧回数
danielchen
NXP TechSupport
NXP TechSupport

HI Chris:

Thank you for reporting this, it is always helpfully to receive customer's feedback.

Daniel

0 件の賞賛
返信