MQX support for Vybrid QSPI1

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MQX support for Vybrid QSPI1

Jump to solution
1,097 Views
nancyb
Contributor III

When will MQX support QSPI1 on Vybrid? Are there issues that prevent cloning the QSPI0 support to support QSPI1?

Regards,

Nancy

0 Kudos
Reply
1 Solution
937 Views
nancyb
Contributor III

Hi RadekS,


I found the problem:we use a tailored MQX 4.1 and QSPI1 was edited out. When I looked at my local MQX 4.1 installation I see the missing support.

Now to add it back to our official version.

Thank you for your help.

Regards,

Nancy

View solution in original post

0 Kudos
Reply
3 Replies
937 Views
RadekS
NXP Employee
NXP Employee

Hi Nancy,

there should not be any issue with QSPI1.

QSPI driver include low level driver supports QSPI1.

twrvf65gs10 contains two Flash chips connected to QSPI0_A and QSPI0_B.

vybrid_autoevb contains three Flash chips connected to QSPI0_A, QSPI0_B and QSPI1.

Do you know about any specific issue with QSPI1?


Have a great day,
RadekS

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply
938 Views
nancyb
Contributor III

Hi RadekS,


I found the problem:we use a tailored MQX 4.1 and QSPI1 was edited out. When I looked at my local MQX 4.1 installation I see the missing support.

Now to add it back to our official version.

Thank you for your help.

Regards,

Nancy

0 Kudos
Reply
937 Views
RadekS
NXP Employee
NXP Employee

Thank you for your clarification.

Now it make sense.

0 Kudos
Reply