MQX codesize tool not working?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MQX codesize tool not working?

ソリューションへジャンプ
1,529件の閲覧回数
lfschrickte
Contributor IV

Hi,

I'm trying to use the codesize tool available in the MQX 4.1 tools folder. However the html output gives me no information, as in the following image:

codesize_report.png

All itens are as above, with an '-' symbol. This is the command I'm using and the stdout output:

codesize_cmd.png

Do you have any idea on why this could be happening? I've tried searching another threads here without success.

Thank you!

Luiz Fernando

タグ(3)
0 件の賞賛
返信
1 解決策
1,442件の閲覧回数
RadekS
NXP Employee
NXP Employee

It should work.

However: Are you sure that you used CW compiler? GCC is currently not supported by this tool.

CW compiler/linker typically generate *.xMap file instead of *.map file.


Best Regards,
RadekS

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
1,443件の閲覧回数
RadekS
NXP Employee
NXP Employee

It should work.

However: Are you sure that you used CW compiler? GCC is currently not supported by this tool.

CW compiler/linker typically generate *.xMap file instead of *.map file.


Best Regards,
RadekS

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信
1,442件の閲覧回数
lfschrickte
Contributor IV

Hi,

I can't test if it will work as a change of toolchain now will be hard, but you're right: I'm using GCC and haven't realized it is not supported!

Hope I can find something similar that works with gcc soon!

Thanks very much!

Luiz Fernando

0 件の賞賛
返信