MQX Vybrid support

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

MQX Vybrid support

4,110 次查看
POSterminalPCI_
Contributor II

Dear Sir/Madam,

Hello,

Is MQX available for Vybrid processors?. If not when it will be available?

Is there ISO 7816 support for MQX?

Best regards.

Mehmet Ali Ipin

标签 (1)
标记 (1)
5 回复数

3,012 次查看
c0170
Senior Contributor III

Hello Mehmet Ali Ipin,

VYBRID processors are going to be supported in next MQX release which should be released in Q2 2013.

Regards,

MartinK

3,012 次查看
POSterminalPCI_
Contributor II

Dear Martin,

Thank you for your answer,

Is it for only Cortex M4 or, Cortex A5-specially VF3XX also supported?

Thanks and best regards.

0 项奖励
回复

3,012 次查看
c0170
Senior Contributor III

Hello,

VF6XX will be supported in the MQX.

Regards,

MartinK

0 项奖励
回复

3,012 次查看
JohnGoodman
Contributor I

So does that means MQX will support VF5XX that has a Cortex-A5 only?

0 项奖励
回复

3,012 次查看
hongtranduc
Contributor II

To be more specific, the MQX is supported Cortex-M4 already, and Cortex-A5 will be supported in this year release.