MQX UVC(USB Video Class) driver

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MQX UVC(USB Video Class) driver

2,912件の閲覧回数
ToddF
Contributor I

I am looking for a UVC (USB video class) driver to use with the MCF5225X family of parts. Is anyone aware of a UVC driver that would allow me to connect a USB webcam to a MCF5225X part running MQX?

 

Thanks, Todd

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

1,646件の閲覧回数
JuroV
NXP Employee
NXP Employee

Hello,

 

as MQX does not still support isochronous transfers for KHCI and EHCI low level drivers, it is not possible to connect USB video-class videorecorder to the MQX-host running MCU. The UVC driver is also not written yet.

0 件の賞賛
返信

1,646件の閲覧回数
mwsealey
Contributor II

What about if configuring for UVC camera device (configuring the Kinetis so it is the microcontroller attached to camera, forwarding video data to a PC or other host)?

 

Is there support for the right features in the stack already?

0 件の賞賛
返信