MQX UVC(USB Video Class) driver

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MQX UVC(USB Video Class) driver

2,907 Views
ToddF
Contributor I

I am looking for a UVC (USB video class) driver to use with the MCF5225X family of parts. Is anyone aware of a UVC driver that would allow me to connect a USB webcam to a MCF5225X part running MQX?

 

Thanks, Todd

Labels (1)
0 Kudos
Reply
2 Replies

1,641 Views
JuroV
NXP Employee
NXP Employee

Hello,

 

as MQX does not still support isochronous transfers for KHCI and EHCI low level drivers, it is not possible to connect USB video-class videorecorder to the MQX-host running MCU. The UVC driver is also not written yet.

0 Kudos
Reply

1,641 Views
mwsealey
Contributor II

What about if configuring for UVC camera device (configuring the Kinetis so it is the microcontroller attached to camera, forwarding video data to a PC or other host)?

 

Is there support for the right features in the stack already?

0 Kudos
Reply