MQX RTOS to boot Linux?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MQX RTOS to boot Linux?

1,818 Views
dry
Senior Contributor I

Is it possible load and execute Linux kernel from MQX? Is there an MQX based bootloader that ran launch Linux? I know there is RedBoot (based on eCos RTOS) which can do it

0 Kudos
Reply
3 Replies

1,563 Views
soledad
NXP Employee
NXP Employee

Hello,

Check the below thread and please let me know if this helps!!

Using U-boot as MQX bootloader


Have a great day,
Sol

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

1,563 Views
dry
Senior Contributor I

Hi soledad,

Well actually I had this as an under-question, I wanted to know if I can avoid using U-boot.

What I would want is a bootloader (hopefully based on MQX.. (what does MQX use to load itself, I havent studied) which can load MQX

or Linux, and be royalty free or non restrictive license so that one can modify the sources without releasing custom changes.

0 Kudos
Reply

1,563 Views
soledad
NXP Employee
NXP Employee

Hi,

Unfortunately we at this moment we don't have a solution like you need.

Sorry for any inconvenience.


Have a great day,
Sol

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply