MQX RTCS HTTPSRV + Internet Explorer 11 problem

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MQX RTCS HTTPSRV + Internet Explorer 11 problem

1,232件の閲覧回数
rafaelmartinez
Contributor I

Hi,

I have a web server running in a MCF52259 microprocessor with MQX Rev. 3.8. The web browser requests temperature data using a cgi script that polls the microprocessor once per second. The cgi script polling works properly when using Chrome or Firefox, but when I use Internet Explorer 11 the microprocessor can not perform other tasks for 1 second when polled by the cgi script.  Basically, the microprocessor stalls for 1 second.  I have not been able to found the problem, but I have noticed that if change the  html web page code to issue two cgi requests back-to-back (without any delay between them) the problem is solved. I have also noticed that if I change from a static public IP address (192.51.x.x) to a private IP address like 192.168.x.x or 10.x.x.x the problem is solved. Is there any MQX setup that would you recommend to change in order to solve this issue? I have changed the max_sessions from 2 to 6 but the problem was not solved. Below is my current setup. Thank for your help.

    _RTCSPCB_init = 4;

    _RTCSPCB_grow = 2;

    _RTCSPCB_max = 6;

    _RTCS_msgpool_init = 4;

    _RTCS_msgpool_grow = 2;

    _RTCS_msgpool_max  = 8;

    _RTCS_socket_part_init = 4;

    _RTCS_socket_part_grow = 2;

    _RTCS_socket_part_max  = 6;

    _RTCSTASK_stacksize = 3500;

    RTCS_create();

    RTCS_selectall(5000);

        // Using setup from MQX example server

        params = httpd_default_params(NULL);

        params->root_dir = (HTTPD_ROOT_DIR_STRUCT*)root_dir;

        params->index_page = "\\index.html";

        params->max_ses    = 2;

ラベル(1)
0 件の賞賛
返信
1 返信

1,048件の閲覧回数
soledad
NXP Employee
NXP Employee

Hello Rafael,

MQX 3.8 version has bugs that there were fixed on the new releases.Could you please migrate to MQX v4.2?

Have a great day,
Sol

0 件の賞賛
返信