MQX Lite Driver functionality (Enable / Disable Interrupts)

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

MQX Lite Driver functionality (Enable / Disable Interrupts)

跳至解决方案
1,544 次查看
lokuate
Contributor III

Hello,

I've found the MQX Lite driver model is different than MQX, MQX Lite drivers are generated by Processor Expert with a pre-determined functionality and are not intended to be messed with.

My application requires me to Disable / Enable the a UART (SCI / AS) port every period of time, and I cannot find that functionality in the P.E. Driver, how can I go about obtaining this functionality.

There's a _int_disable() function in MQX Lite that disables all interrupt up to the current task priority, that is not exactly what I want or need.

I hope somebody can help me get out of this jam, I'm new with MQX.

I used to work with FreeRTOS where there's a xUARTdisable(UART1handle); function that does the trick.

Kindest Regards,

Carlos

0 项奖励
回复
1 解答
1,248 次查看
petr_uhlir
NXP Employee
NXP Employee

Hello Carlos,

if you are using Serial_LDD driver you can use Enable and Disable methods. Both are not generated by default so you have to switch to Advanced or Expert mode and set Value to "generate code"

AS1.PNG

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,249 次查看
petr_uhlir
NXP Employee
NXP Employee

Hello Carlos,

if you are using Serial_LDD driver you can use Enable and Disable methods. Both are not generated by default so you have to switch to Advanced or Expert mode and set Value to "generate code"

AS1.PNG

0 项奖励
回复